• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Fault and Normal Diagnostic Considerations for Smart High Side Switches

    • SLVAEX0 October   2020 TPS1H000-Q1 , TPS1H100-Q1 , TPS1H200A-Q1 , TPS1HA08-Q1 , TPS1HB16-Q1 , TPS1HB50-Q1 , TPS2HB16-Q1 , TPS2HB50-Q1 , TPS4H000-Q1 , TPS4H160-Q1

       

  • CONTENTS
  • SEARCH
  • Fault and Normal Diagnostic Considerations for Smart High Side Switches
  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2Normal Operation Diagnostics
    1. 2.1 Configuring Diagnostics With SEL/SELx Pin
      1. 2.1.1 Diagnostics Select Pin: SEL1
      2. 2.1.2 Diagnostics Select Pin: SELx
    2. 2.2 Operating Current Measurements Using the SNS/CS Pin
      1. 2.2.1 Internal/External Factor: Load Current Through Device
      2. 2.2.2 External Factor: Analog-to-Digital Converter (ADC)
      3. 2.2.3 External Factor: Probe Ground Termination
      4. 2.2.4 External Factor: Component Tolerances
    3. 2.3 Device Temperature on the Sense (SNS) Pin
  5. 3Fault State Diagnostics
    1. 3.1 Fault Behavior Configurations: Latch/THER/Delay Pin
      1. 3.1.1 Latch Pin
      2. 3.1.2 THER Pin
      3. 3.1.3 Delay Pin
    2. 3.2 Open Load Fault
    3. 3.3 Short to Battery Fault
    4. 3.4 Thermal Shutdown
    5. 3.5 Loss of Ground or Power Supply
    6. 3.6 Summary
  6. 4References
  7. IMPORTANT NOTICE
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
APPLICATION NOTE

Fault and Normal Diagnostic Considerations for Smart High Side Switches

Abstract

The operation of a high side switch becomes smoother, smarter, and enhanced when adding features such as diagnostics and fault reporting. Diagnostics and fault reporting are key features in high side switches to protect power supplies and loads such as LEDs or motors safe while keeping the switch intact. The following application report goes over the diagnostics and fault reporting that are provided in TI’s Smart High Side Switch solutions in both normal and fault conditions such as accurate current sensing, short-to-GND detection, and open load detection. Using this document, designers can take advantage of each advanced function and make the most of TI’s high side switch in their application.

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

High Side Switches are used and seen most commonly in automotive and industrial applications. High side switches have applications where providing power to off-board loads are essential, providing a point of disconnect between the system, supply, and the load. High-side switches can provide diagnostics during normal operation, such as load current measurement and device temperature monitoring. With load current measurements, the system is able to take measurements of the output current by correlating it with a voltage based output. With device temperature monitoring, the system is able to monitor the internal junction temperature of the switch as it increases during operation using a voltage based output. High side switches also provide diagnostics for faults that can alert when open loads, short-to-GND, loss of battery, or thermal shutdown occur. Each fault brings efficiency to the system by allowing features that help monitor down time and ways to ensure current can continue to be drawn through the switch.

2 Normal Operation Diagnostics

Aside from simple on-off operation, most TI smart high-side switch devices come with diagnostics that help monitor regular operation. Some devices have pins that allow measuring the operating load current on the Current Sense [CS] pin. As the device is best kept operating below a certain temperature threshold, the device junction temperature may also be of interest when monitoring device operation. The following sections discuss how to configure the different operations on devices that are able to and also how to optimize current measurements. Table 2-1 lists the devices that are able to measure load current or both device temperature and load current by using their Current Sense (CS) or Sense (SNS) pins.

Table 2-1 Devices With Current Sense or Sense Pins
Feature Devices
Current Sensing: CS or Current Sense (ISNS) Pin TPS1H100-Q1, TPS27S100, TPS2H160-Q1, TPS4H160-Q1, TPS2H000-Q1, TPS4H000-Q1
Current and Temperature Monitoring: SNS Pin TPS1HA08, TPS1HBxx, TPS2HBxx
No Current Sensing or Temperature Monitoring TPS1H200A-Q1, TPS1H000A-Q1

2.1 Configuring Diagnostics With SEL/SELx Pin

For devices that have a configurable output pin for measuring either the operating load current or the device temperature, there are pins that need to be configured to the appropriate logic values to see the respective output. These are the Select High and Low pins (SEL, SHE) or the Select 1 or Select 2 pins (SELx) pins. By pulling either of these pins to the pin’s high or low logic, the diagnostic output is configured to either the device temperature or the operating load current. Table 2-2 shows the different devices and their corresponding SEL/SELx pin.

Table 2-2 Devices With Select Pins
Feature Devices
SEL and SEH pin TPS4H160-Q1, TPS2H000-Q1, TPS4H000-Q1
SELx pins TPS1HA08-Q1, TPS1HB16-Q1, TPS1HB35-Q1, TPS1HB50-Q1, TPS2HB16-Q1, TPS2HB50-Q1

2.1.1 Diagnostics Select Pin: SEL1

Devices such as the TPS1HB16 have a single SEL1 pin that can be configured with a high or low signal. It acts as the diagnostics select pin. Depending on its state, one of two outputs will be measurable from the sense output pin SNS. The first is load current, which allows the SNS pin to output a voltage signal that reflects the load current that the switch is outputting. The second is the device’s junction temperature. The junction temperature is the internal temperature of the switch and is important to monitor to ensure the device remains below the thermal thresholds. These different output configurations are shown in Table 2-3.

Table 2-3 SNS Pin Output Based on SEL1 Pin State
SEL1 Pin State SNS Pin Output
Low Load Current
High Device Temperature

2.1.2 Diagnostics Select Pin: SELx

For devices that have multiple SEL pins such as the TPS1HA08, the device is able to be configured in three ways: device temperature, load current, or supply voltage. As with the single SEL pin devices, device temperature allows for measuring the internal junction temperature and the load current measurement allows for a proportionate voltage signal that reflects the load current. An additional setting allows for monitoring the supply voltage that is supplying power to the output, which is helpful in applications where a battery is involved such as in the automotive industry. For devices with multiple channels, additional SEL pins are used to select which channel to monitor.

Table 2-4 shows the different diagnostics that are used in the SELx pins on the TPS1HA08-Q1 and how to configure them. Table 2-5 shows the configurations that available on the SELx pins on the TPS2HB16 and the settings associated with them.

Table 2-4 SELx Configuration for the TPS1HA08-Q1
SEL1 State SEL2 State SNS Pin Output
Low Low Load Current
Low High No Diagnostics
High Low Device Temperature
High High Supply Voltage
Table 2-5 SELx Configuration on the TPS2HB16-Q1
SEL1 State SEL2 State SNS Pin Output
Low Low Channel 1 Load Current
Low High Channel 2 Load Current
High Low Device Temperature
High High N/A

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale