SLUP413A May   2024  – April 2026 TPS53689T

 

  1.   1
  2.   Abstract
  3. Introduction
  4. Converter Transient Response
  5. Magnetics
  6. TLVR Topology Operating Principles
    1. 4.1 Steady-State Operation
    2. 4.2 Load Transient Step-Up
    3. 4.3 Load Transient Step-Down
    4. 4.4 LC Inductor Selection
    5. 4.5 Steady-State Ripple
  7. Power Loss and Efficiency
  8. Phase Multiplication
  9. PCB Layout
  10. TLVR-Optimized Components
  11. Example Side-by-Side Design
  12. 10Summary
  13. 11Additional Resources

Steady-State Operation

Figure 11 shows a typical TLVR converter schematic, with important nodes, voltages and currents labeled. Figure 12 illustrates the steady-state operating waveforms of a TLVR converter, with four phases shown. In this example, the pulses from adjacent phases do not overlap in time. There is no maximum duty-cycle requirement for the TLVR topology. The same principles apply for higher-duty-cycle applications where pulses do overlap in time.

Figure 12 shows the voltage and current waveforms of the LC of the secondary-side loop, switch nodes of all four phases, and the primary-side current of phase 4 (IPRI4). For clarity, this figure includes labels for the three distinct states of operation.

The most important relationships are those of the LC loop and its influence on IPRI and ISUM.

 Steady-state
                        topology.
Four-phase example, no pulse overlap
Figure 11 Steady-state topology.
 Steady-state
                        waveforms.
Four-phase, no pulse overlap
Figure 12 Steady-state waveforms.

The magnetizing voltage for each phase is similar to that of a buck converter. Equation 6 applies to phase on, and Equation 7 applies to phase off. The magnetizing inductance always follows the fundamental inductor relationship shown in Equation 8:

Equation 6. Δ V L m , i = V I N - V O U T
Equation 7. Δ V L m , i = - V O U T
Equation 8. I L M = Δ V L m L m

The voltage across the LC is always equal to the sum of the magnetizing voltages across all phases, as shown in Equation 9. LC itself always follows the fundamental inductor relationship, expressed by Equation 10:

Equation 9. Δ V L C = V L m 1 + V L m 2 +
Equation 10. I L C = Δ V L C L C

The IPRI for each phase is equal to the sum of its magnetizing current and ILC, expressed in Equation 11. ISUM is the sum of the primary currents from all phases, expressed by Equation 12:

Equation 11. I P R I , i = I L m , i + I L C
Equation 12. I S U M = I P R I 1 + I P R I 2 +

Table 1 summarizes the state of each of the relevant voltages and currents shown in Figure 12, with respect to the derivation of IPRI4 shown in the plot.

Table 1 Four-phase example, steady-state voltages and currents.
Parameter State 1
Phase 4 on, phases 1, 2 and 3 off
State 2
All phases off
State 3
Phase 4 and two others off, one of the other phases is on
VSW1 0 V 0 V One phase is equal to VIN and the other two are equal to 0 V.
VSW2 0 V 0 V
VSW3 0 V 0 V
VSW4 VIN 0 V 0V
ΔVLM1 –VOUT –VOUT One phase is equal to VIN – VOUT and the other two are equal to –VOUT
ΔVLM2 –VOUT –VOUT
ΔVLM3 –VOUT –VOUT
ΔVLm4 VIN – VOUT –VOUT –VOUT
ILm4 Increasing Decreasing Decreasing
ΔVLC Sum of ΔVLM1–4 Sum of ΔVLM1–4 Sum of ΔVLM1–4
ILC Increasing Decreasing Increasing
IPRI4 Increasing Decreasing faster Decreasing slower