SLUAA80 November   2020 TPS40322

 

  1.   Trademarks
  2. 1Introduction
  3. 2Circuit Description
    1. 2.1 Calculation for VOUT Settings
  4. 3Setup TPL0102-100 EVM
    1. 3.1 Connection Block Diagram
    2. 3.2 Software GUI Setup
  5. 4Conclusion

Software GUI Setup

Utilize the bqStudio GUI for read/write the I2C commands to I2C slave device. Use the following procedure to set up the bqStudio GUI to control the TPL0102-100EVM and adjust as a variable resistor. Figure 3-5 second (fourth) Figure 3-6

  1. Open BqStudio, select Charger, and click the Next button
    GUID-20201106-CA0I-JKMN-CJLJ-MWRGB2CX73VB-low.png Figure 3-3 Charger Device Type.
  2. Select the bq24773.bqz target and click the Finish button
    GUID-20201106-CA0I-LTQP-VMWV-2D3VLWXH29ST-low.png Figure 3-4 bq24773.bqz Target.
  3. Select the Advanced Comm tab
    GUID-20201106-CA0I-N2TZ-VHKC-T7K7P2DB9TRL-low.png Figure 3-5 Advanced Comm tab.
  4. Read/Write I2C command to TPL0102-100 EVM

    illustrates using the Advanced Comm tab to set the device address to 0xA0h and read/write 1 byte data from and to the register 0x00h for accessing the Wiper Resistance Register of Potentiometer A.

    GUID-20201106-CA0I-WFWJ-D7M8-6CNWS4LL5FGQ-low.png Figure 3-6 Byte Read/Write Settings.