SLUAA80 November   2020 TPS40322

 

  1.   Trademarks
  2. 1Introduction
  3. 2Circuit Description
    1. 2.1 Calculation for VOUT Settings
  4. 3Setup TPL0102-100 EVM
    1. 3.1 Connection Block Diagram
    2. 3.2 Software GUI Setup
  5. 4Conclusion

Setup TPL0102-100 EVM

RH and RL in Figure 2 are presenting the RHW, RWL of the TPL0102 device. An I2C master connects to the TPL0102 and is required to get control the RHW, RWL of the TPL0102. Figure 3-1 shows a connection example which uses the TI EV2400 tool as a I2C master to set the RHW, RWL values via the bqStudio GUI.