SLUAA45 April 2020 BQ27Z561
The gauge gets cell resistance from interpolating Ra table, which inevitably leads to some error in SOC. The error could be large at low temperature and heavy load, especially near the end of discharge when resistance changes quickly, which may cause SOC jump issue.
Fast Resistance Scaling is an algorithm that improves SOC convergence to 0% by scaling cell resistance as (Rnew / Rold), where Rnew is the most recent measured resistance and Rold is the interpolated resistance at present DOD. After a scale is calculated, an IT simulation is triggered to utilize the new resistance information.