SLLU146D May 2011 – June 2025
The EVM board can be used to test the WAKE functionality of the TUSB73X0. By default, the EVM is not configured to support wake testing. Configure the EVM according to the following if WAKE is required:
For some motherboards, WAKE from a PCIe slot is not supported or is only supported on PCIE X1 slots. Make sure to use a motherboard that supports WAKE from any PCIe slot.