SLIU023 June 2021
This section describes the test setup for the evaluation of the TLC6A598EVM board. Table 2-1 shows the EVM connectors and test points.
| Reference Designator | Function |
|---|---|
| J1 | VCC |
| J2 | GND for VCC |
| J3 | VDD |
| J4 | GND for VDD |
| J5 | USB2ANY Connector |
| J6 | Outputs connector for TLC6A598 |
| J7 | Outputs connector for Relays |
| TP1 | Test point for VCC |
| TP2 | Test Point for VDD |
| TP3, TP4, TP5 | GND Test Point |
The following equipment are required for the test setup:
To evaluate the TLC6A598EVM board, the USB2ANY interface adapter provided by TI is recommended here. Please download and install the USB2ANY Explorer Software on the computer.
Figure 2-1 shows the test bench setup for the evaluation of the TLC6A598EVM board.
Set the input voltage power supply 1 to 5 V and the current limit to 0.3 A. Turn off the power supply 1. Connect the power supply 1 to the J1 and J2 connectors with the positive terminal of the supply connected to VCC (J1) and the negative terminal of the supply connected to GND (J2). Set the input voltage power supply 2 to 24 V and the current limit to 1 A. Turn off the power supply 2. Connect the power supply 2 to the J3 and J4 connectors, with the positive terminal of the supply connected to VDD (J3) and the negative terminal of the supply connected to GND (J4).
Connect the USB2ANY with Edge cable to J5 and connect USB2ANY to the PC with USB cable.
With above setup and connections completed, turn on the power supply 1 and 2. Then open the USB2ANY Explorer Software and the software will show as Figure 2-2.
Click the 'Select Interface' button and choose the 'GPIO' and 'SPI' as Figure 2-3 and click the 'Close' button.
Click the 'GPIO' button and configure the GPIO3 as Figure 2-4. If you cannot see the 'GPIO' button, please adjust the display scale of the PC to 100%.
Click the 'SPI' button and configure the SPI interface as Figure 2-5:
In the 'Write date' command window, write 'FF' and click 'Write/Read' button as Figure 2-6:
Then, the eight relays K1 to K8 will turn on and the eight Green LEDs D1 to D8 will turn on accordingly.
Please refer to the TLC6A598 data sheet for additional functional tests.