SLAZ742E July 2023 – December 2025 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
SRAM Module
Functional
SRAM Error address returns value with the most significant byte missing
SRAM DEDERRADDR will return the wrong value, the most significant byte gets truncated. For example a parity error at 0x20001234 would return the parity error address as 0x00001234.
Perform a bit wise OR operation with the SRAM origin and the SYSCTRL->DEDERRADDR return value, when an SRAM DED or SRAM Parity fault is triggered. View the device datasheet for SRAM Memory start locations, the linker file will also have the origin of the SRAM address.