SLAU866 November 2021 DAC43204 , DAC53202 , DAC53204 , DAC63202 , DAC63204
The Basic DAC subpage shown in Figure 3-5 provides an interface to quickly power up, select the reference and output span, and program the output voltage or current for the respective DACx3204 device. When VDD is applied, the DACx3204 device starts up in Hi-Z power-down mode by default. The Basic DAC subpage also provides controls to configure the GPIO pin on the respective DACx3204 device, and control the two GPIO outputs of the DAC63204EVM onboard controller. The register settings can be programmed or retrieved using the Program NVM or Reload NVM checkboxes, respectively.
Figure 3-5 Basic DAC Subpage