SLAA954 August   2020  – MONTH  TAS2563

 

  1.   Abstract
  2.   Trademarks
  3. 1End System Integration
    1. 1.1 Step 1: Exporting Binary and Configuration Files
    2. 1.2 Step 2: Configuration Selection
    3. 1.3 Step 3: Snapshot Selection
  4. 2Factory Test and Calibration (FTC)
    1. 2.1 Step 4: Pass/Fail Limits
    2. 2.2 Step 5: Configuration Summary
  5. 3Device Driver Integration
    1. 3.1 Case 1 : Initialization
    2. 3.2 Case 2: Power up
    3. 3.3 Case 3: New Configuration
    4. 3.4 Case 4: New Configuration and PLL
    5. 3.5 Case 5: New Configuration and Program
  6. 4Summary

Step 3: Snapshot Selection

Assign the tuning snapshot previously saved during “Tuning and Audio Processing” page to each configurations. Please name the file folder and assign the path to save the files. In addition, Various data can be read through the ASI Record Channel (shown in Figure 1-5) to suit the system application. The ASI Record Channel can be accessed by the gear icon in the top right corner. An example application of "Audio In & Out" in ASI Record Channel can be used for echo reference. Select “Next” to begin configuring the .ftcfg file for factory test calibration.

GUID-20200721-CA0I-HVT8-XVQS-ZGJ8BBGVZMSS-low.pngFigure 1-4 Snapshot Selection.
GUID-20200721-CA0I-SDM6-GGTM-F2J91G02PNCM-low.pngFigure 1-5 ASI Record Channel Selection.

Note:

Steps 1 to 4 cover the settings for the binary file. Before users are able to export the binary file, please continue to the next section to complete the FTC configuration.