SFFSAX5 December   2025 TCAN1476-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 VSON (14, DMT) Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 TCAN1476-Q1 (VSON (14, DMT) Package)
    2. 4.2 TCAN1476V-Q1 (VSON (14, DMT) Package)
  7. 5Revision History

TCAN1476-Q1 (VSON (14, DMT) Package)

Figure 4-1 shows the TCAN1476-Q1 pin diagram for the VSON (14, DMT) package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TCAN1476-Q1 datasheet.

TCAN1476-Q1 TCAN1476V-Q1 Pin Diagram (VSON (14, DMT) Package)Figure 4-1 Pin Diagram (VSON (14, DMT) Package)
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No. Description of Potential Failure EffectsFailure Effect Class
TXD11The CAN1 driver enters dominant timeout, disabling the driver. Data cannot be transmitted on the CAN1 bus.B
GND12None.D
VCC13The CAN1 transceiver becomes unpowered and a high system-level supply current potentially occurs.B
RXD14By default, the RXD pin is high-side FET ON. With a pin short-circuit to ground, a direct path forms between supply and ground, causing high current flow.A
TXD25The CAN2 driver enters dominant timeout, disabling the driver. Data cannot be transmitted on the CAN2 bus.B
GND26None.D
VCC27The CAN2 transceiver becomes unpowered and a high system-level supply current potentially occurs.B
RXD28By default, the RXD pin is high-side FET ON. With a pin short-circuit to ground, a direct path forms between supply and ground, causing high current flow.A
CANL29The VCANL(R) specification is violated. The EMC performance of the transceiver potentially degrades.C
CANH210The device cannot drive a dominant signal to the CAN2 bus, so communication on the CAN2 bus is not possible.B
STB211The STB2 pin is stuck low, so the CAN2 transceiver is unable to enter low-power mode.B
CANL112The VCANL(R) specification is violated. The EMC performance of the transceiver potentially degrades.C
CANH113The device cannot drive a dominant signal to the CAN1 bus, so communication on the CAN1 bus is not possible.B
STB114The STB1 pin is stuck low, so the CAN1 transceiver is unable to enter low-power mode.B
Thermal Pad-None.D
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin NamePin No. Description of Potential Failure EffectsFailure Effect Class
TXD11The TXD1 pin defaults high; the CAN1 driver is always recessive and unable to transmit data.B
GND12The CAN1 transceiver is not powered.B
VCC13The CAN1 transceiver is not powered.B
RXD14There is no RXD1 pin connection to the MCU. The MCU is unable to read data from the CAN1 bus using the RXD1 pin.B
TXD25The TXD2 pin defaults high; the CAN2 driver is always recessive and unable to transmit data.B
GND26The CAN2 transceiver is not powered.B
VCC27The CAN2 transceiver is not powered.B
RXD28There is no RXD2 pin connection to the MCU. The MCU is unable to read data from the CAN2 bus using the RXD2 pin.B
CANL29The device cannot drive a dominant signal on the CAN2 bus, so communication on the CAN2 bus is not possible.B
CANH210The device cannot drive a dominant signal on the CAN2 bus, so communication on the CAN2 bus is not possible.B
STB211The STB2 pin defaults high; the CAN2 transceiver is stuck in low-power mode.B
CANL112The device cannot drive a dominant signal on the CAN1 bus, so communication on the CAN1 bus is not possible.B
CANH113The device cannot drive a dominant signal on the CAN1 bus, so communication on the CAN1 bus is not possible.B
STB114The STB1 pin defaults high; the CAN1 transceiver is stuck in low-power mode.B
Thermal Pad-None.D
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure EffectsFailure Effect Class
TXD11GND1The CAN1 driver enters dominant timeout, disabling the driver. Data cannot be transmitted on the CAN1 bus.B
GND12VCC1The CAN1 transceiver becomes unpowered, and high ICC current flow is possible.B
VCC13RXD1The output of the RXD1 pin becomes stuck high. The MCU is unable to receive data from the CAN1 bus using the RXD1 pin.B
RXD14TXD2The output of the RXD1 pin reflects the input to the TXD2 pin, a separate CAN channel. Information from the CAN1 bus is not received correctly by the MCU, or information from the MCU to the CAN2 bus is potentially disrupted, or both.B
TXD25GND2The CAN2 driver enters dominant timeout, disabling the driver. Data cannot be transmitted on the CAN2 bus.B
GND26VCC2The CAN2 transceiver becomes unpowered and a high system-level supply current potentially occurs.B
RXD28CANL2The messages on the RXD2 pin are corrupted by the CANL2 pin. The reception of data from the CAN2 bus using the RXD2 pin is not possible. IOS current is potentially reached.B
CANL29CANH2The CAN2 bus becomes stuck recessive and no communication is possible. IOS current is potentially reached when the CAN2 driver is transmitting.B
CANH210STB2The CAN2 transceiver potentially turns off when a dominant signal is driven on the CAN2 bus. The device potentially does not enter or stay in the desired mode for the CAN2 bus.B
STB211CANL1The CAN2 transceiver potentially turns off when the CAN1 bus is recessive. The device potentially does not enter or stay in the desired mode for the CAN2 bus.B
CANL112CANH1The CAN1 bus becomes stuck recessive and no communication is possible. IOScurrent is potentially reached when the CAN1 driver is transmitting.B
CANH113STB1The CAN1 transceiver potentially turns off when a dominant signal is driven on the CAN1 bus. The device potentially does not enter or stay in the desired mode for the CAN1 bus.B
Table 4-5 Pin FMA for Device Pins Short-Circuited to VCC
Pin NamePin No. Description of Potential Failure EffectsFailure Effect Class
TXD11The TXD1 pin becomes stuck high. The device is unable to transmit data on the CAN1 bus.B
GND12The CAN1 transceiver becomes unpowered, and high ICC is possible.B
VCC13NoneD
RXD14The RXD1 pin becomes stuck high. The MCU is unable to read data from the CAN1 bus using the RXD1 pin.B
TXD25The TXD2 pin becomes stuck high. The device is unable to transmit data on the CAN2 bus.B
GND26The CAN2 transceiver becomes underpowered, and high ICC is possible.B
VCC27NoneD
RXD28The RXD2 pin becomes stuck high. The MCU is unable to read data from the CAN2 bus using the RXD2 pin.B
CANL29The device cannot drive a dominant signal to the CAN2 bus, so no communication is possible. The CAN2 bus potentially becomes stuck recessive during the fault.B
CANH210The VCANL(R) specification is violated. The EMC performance of the transceiver potentially degrades.C
STB211The STB2 pin is stuck high. The CAN2 transceiver becomes stuck in low-power mode.B
CANL112The device cannot drive a dominant signal to the CAN1 bus, so no communication is possible. The CAN1 bus potentially becomes stuck recessive during the fault.B
CANH113The VCANL(R) specification is violated. The EMC performance of the transceiver potentially degrades.C
STB114The STB1 pin is stuck high. The CAN1 transceiver becomes stuck in low-power mode.B
Table 4-6 Pin FMA for Device Pins Short-Circuited to VBAT
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
TXD11An absolute maximum violation occurs. The device is potentially damaged. The device potentially cannot transmit data on the CAN1 bus.A
GND12The device becomes unpowered. High IBAT current is possible.B
VCC13An absolute maximum violation occurs. The device is potentially damaged. The CAN1 bus potentially cannot communicate.A
RXD14An absolute maximum violation occurs. The device is potentially damaged. The MCU potentially cannot receive data from the CAN1 bus.A
TXD25An absolute maximum violation occurs. The device is potentially damaged. The device potentially cannot transmit data on the CAN2 bus.A
GND26The device becomes unpowered. High IBAT current is possible.B
VCC27An absolute maximum violation occurs. The device is potentially damaged. The CAN1 bus potentially cannot communicate.A
RXD28An absolute maximum violation occurs. The device is potentially damaged. The MCU potentially cannot receive data from the CAN2 bus.A
CANL29The CAN2 bus becomes stuck recessive. No communication is possible. IOS current is potentially reached.B
CANH210The VCANL(R) specification is violated. The EMC performance of the transceiver potentially degrades.C
STB211An absolute maximum violation occurs. The device is potentially damaged. The CAN2 transceiver becomes stuck in low-power mode.A
CANL112The CAN2 bus becomes stuck recessive. No communication is possible. IOS current is potentially reached.B
CANH113The VCANL(R) specification is violated. The EMC performance of the transceiver potentially degrades.C
STB114An absolute maximum violation occurs. The device is potentially damaged. The CAN1 transceiver becomes stuck in low-power mode.A