SFFSA17 October 2024 TCAN1473A-Q1
This section provides a failure mode analysis (FMA) for the pins of the TCAN1473A-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-7 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
| Class | Failure Effects |
|---|---|
| A | Potential device damage that affects functionality. |
| B | No device damage, but loss of functionality. |
| C | No device damage, but performance degradation. |
| D | No device damage, no impact to functionality or performance. |
Figure 4-1 shows the TCAN1473A-Q1 pin diagram for the 14-pin SOIC (D) and 14-pin SOT (DYY) packages. Figure 4-2 shows the TCAN1473A-Q1 pin diagram for the 14-pin VSON (DMT) package. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TCAN1473A-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| TXD | 1 | The TXD pin is biased dominant indefinitely. The device enters dominant time-out mode. The device is unable to transmit data. | B |
| GND | 2 | None | D |
| VCC | 3 | The device enters sleep mode. There is a high current draw from the external regulator supplying the VCC pin. | B |
| RXD | 4 | The output of the receiver is biased recessive indefinitely. The host is unable to receive data from the bus. | B |
| VIO | 5 | The device enters sleep mode. The transceiver is passive on the bus. There is a high current draw from the external regulator supplying the VIO pin. | B |
| EN | 6 | The EN pin is biased low. The device is unable to enter normal mode. The device is unable to communicate. | B |
| INH | 7 | The ISUP current is high. The INH pin is potentially damaged and indication from the transition to sleep mode is not available. | A |
| nFAULT | 8 | The nFAULT pin is biased low indefinitely, which indicates a fault indefinitely. | B |
| WAKE | 9 | The WAKE pin is biased low indefinitely and is unable to utilize the local wake-up function. | B |
| VSUP | 10 | The device is not powered. There is a high current flowing from the source supplying VSUP flowing to GND. | B |
| INH_MASK | 11 | The inhibit mask function cannot be used as intended. | B |
| CANL | 12 | There is a violation of the VO(REC) specification. EMC performance is degraded. | C |
| CANH | 13 | The device cannot drive the dominant bit to the bus, communication is not possible. | B |
| nSTB | 14 | The nSTB pin is biased low indefinitely. The transceiver is unable to enter normal mode. The device is unable to communicate. | B |
| Thermal Pad | - | None | D |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| TXD | 1 | The TXD pin defaults to a recessive bias. The device is always recessive and unable to transmit data. | B |
| GND | 2 | The device is not powered. | B |
| VCC | 3 | The device in protected mode. | B |
| RXD | 4 | There is no RXD output, the device is unable to receive data. | B |
| VIO | 5 | The device in protected mode. | B |
| EN | 6 | The EN pin defaults to a logic-low bias. The device is unable to enter normal mode. The device is unable to communicate. | B |
| INH | 7 | None | D |
| nFAULT | 8 | There is no effect on performance, but the device is unable to monitor system faults. | B |
| WAKE | 9 | There is no effect on performance, but the device is unable to utilize the local wake-up function. | B |
| VSUP | 10 | The device is not powered. | B |
| INH_MASK | 11 | The inhibit mask function cannot be used as intended. | B |
| CANL | 12 | The device cannot drive dominant on the bus. The device is unable to communicate. | B |
| CANH | 13 | The device cannot drive dominant on the bus. The device is unable to communicate. | B |
| nSTB | 14 | The nSTB pin defaults to a logic-low bias. The device is unable to enter normal mode. The device is unable to communicate. | B |
| Thermal Pad | - | None | D |
| Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|---|
| TXD | 1 | GND | The TXD pin is biased dominant indefinitely and the device enters dominant time-out mode. The device is unable to transmit data. | B |
| GND | 2 | VCC | The device is in protected mode, the ICC current is high. | B |
| VCC | 3 | RXD | The output of the RXD pin is biased recessive indefinitely. The controller is unable to receive data from the CAN bus. | B |
| RXD | 4 | VIO | The output of the RXD pin is biased recessive indefinitely. The controller is unable to receive data from the CAN bus. | B |
| VIO | 5 | EN | The EN pin is biased high indefinitely. The device is unable to enter the standby and silent modes. | B |
| EN | 6 | INH | There is a violation of the absolute maximum rating on the EN pin (except in sleep mode). The transceiver is potentially damaged. | A |
| nFAULT | 8 | WAKE | There is a potential violation of the absolute maximum rating on the nFAULT pin if WAKE is biased high. The transceiver is potentially damaged. | A |
| WAKE | 9 | VSUP | The WAKE pin is biased high indefinitely, the device is unable to utilize local wake-up function. | B |
| VSUP | 10 | INH_MASK | There is a violation of the absolute maximum rating on the INH_MASK pin. The transceiver is potentially damaged. | A |
| INH_MASK | 11 | CANL | If the INH_MASK pin is at VIO level, the IOS
current is potentially reached; RXD is always recessive. If the INH_MASK pin is at logic low, the O(REC) specifications are violated. EMC performance is degraded. | B |
| CANL | 12 | CANH | The bus is biased recessive. Communication is not possible. The IOS current is potentially reached on the CANH or CANL pin. | B |
| CANH | 13 | nSTB | The driver and receiver turn off when the CAN bus is recessive. The device potentially does not enter normal mode. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| TXD | 1 | There is a violation of the absolute maximum rating. The transceiver is potentially damaged. | A |
| GND | 2 | The device is not powered. The ISUP current is high. | B |
| VCC | 3 | There is a violation of the absolute maximum rating. The transceiver is potentially damaged. | A |
| RXD | 4 | There is a violation of the absolute maximum rating. The transceiver is potentially damaged. | A |
| VIO | 5 | There is a violation of the absolute maximum rating. The transceiver is potentially damaged. | A |
| EN | 6 | There is a violation of the absolute maximum rating. The transceiver is potentially damaged. | A |
| INH | 7 | Minimal current is driven into the INH pin. | D |
| nFAULT | 8 | There is a violation of the absolute maximum rating. The transceiver is potentially damaged. | A |
| WAKE | 9 | The WAKE pin is biased high. The device is unable to utilize the local wake-up function. | B |
| VSUP | 10 | None | D |
| INH_MASK | 11 | There is a violation of the absolute maximum rating. The transceiver is potentially damaged. | A |
| CANL | 12 | The IOS current is potentially reached. The RXD pin is always recessive. | B |
| CANH | 13 | The VO(REC) specification is violated. EMC performance is degraded and communication errors potentially result. | C |
| nSTB | 14 | There is a violation of the absolute maximum rating. The transceiver is potentially damaged. | A |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| TXD | 1 | The TXD pin is biased recessive indefinitely. The device is unable to transmit data. | B |
| GND | 2 | The CAN transmitter is not powered and the device enters sleep mode. There is a high current draw from the external regulator supplying the VCC pin. | B |
| VCC | 3 | None | D |
| RXD | 4 | The output of the receiver is biased recessive indefinitely. The host is unable to receive data from the bus. | B |
| VIO | 5 | The I/O pins operate as 5V input and output pins. The microcontroller is potentially damaged if VCC > VIO. | C |
| EN | 6 | The EN pin is biased high indefinitely. The device is unable to enter the standby and silent modes. | B |
| INH | 7 | There is a violation of the absolute maximum rating on the VCC pin. The INH pin is biased at the VCC voltage. The system potentially does not wakeup. | A |
| nFAULT | 8 | The nFAULT pin is biased high indefinitely. The transceiver is unable to report faults. | B |
| WAKE | 9 | None | D |
| VSUP | 10 | There is a violation of the absolute maximum rating on the VCC pin. | A |
| INH_MASK | 11 | The inhibit mask function is activated when the device enters silent mode. The microcontroller is potentially damaged if VCC > VIO. | B |
| CANL | 12 | The IOS current is potentially reached. The RXD pin is always recessive. | B |
| CANH | 13 | The VO(REC) specification is violated. EMC performance is degraded. | C |
| nSTB | 14 | The nSTB pin is biased high indefinitely. The transceiver is unable to enter the standby and sleep modes. | B |
| Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
|---|---|---|---|
| TXD | 1 | The TXD pin is biased recessive indefinitely. The device is unable to transmit data. | B |
| GND | 2 | The device is not powered. There is a high current draw from the external regulator supplying to the VIO pin. | B |
| VCC | 3 | The I/O pins operate as 5V input and outputs pins. The microcontroller is potentially damaged if VCC > VIO. | C |
| RXD | 4 | The output of the receiver is biased recessive indefinitely. The host is unable to receive data from bus. | B |
| VIO | 5 | None | D |
| EN | 6 | The EN pin is biased high indefinitely. The device is unable to enter the standby and silent modes. | B |
| INH | 7 | There is a violation of the absolute maximum rating on the VIO pin. The INH pin is biased at the VIO voltage. The system potentially does not wakeup. | B |
| nFAULT | 8 | The nFAULT pin is biased high indefinitely. The transceiver is unable to report faults. | B |
| WAKE | 9 | None | D |
| VSUP | 10 | There is a violation of the absolute maximum rating on the VIO pin. | A |
| INH_MASK | 11 | The inhibit mask function is activated when the device enters silent mode. | D |
| CANL | 12 | The IOS current is potentially reached. The RXD pin is always recessive. | B |
| CANH | 13 | The VO(REC) specification is violated. EMC performance is degraded. | C |
| nSTB | 14 | The nSTB pin is biased high indefinitely. The transceiver is unable to enter the standby and sleep modes. | B |