SFFS167B september 2021 – july 2023 ADS117L11 , ADS127L11 , ADS127L21
Figure 4-2 shows the ADS117L11, ADS127L11, and ADS127L21 pin diagram for the WQFN package. For a detailed description of the device pins, see the Pin Configuration and Functions sections in the ADS117L11, ADS127L11 and ADS127L21 data sheets.
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
AINP | 1 | AINP is stuck low. Conversion results are correct only if AINP is tied to DGND in actual use, otherwise conversion results are incorrect. | B |
AINN | 2 | AINN is stuck low. Conversion results are correct only if AINN is tied to DGND in actual use, otherwise conversions results are incorrect. | B |
VCM | 3 | VCM is stuck low. Conversion results are incorrect if actively used for the external driver stage to set the signal common-mode voltage. | B |
REFP | 4 | REFP is stuck low. Conversion results are incorrect. | B |
REFN | 5 | REFN is stuck low. Conversion data are correct only if REFN is tied to DGND in actual use, otherwise conversions results are incorrect. | B |
RESET | 6 | RESET is stuck low. The device is not functional. | B |
CS | 7 | CS is stuck low in four-wire SPI mode. SPI communication is not functional because of inability to control SPI data frames. | B |
CS is stuck low in three-wire SPI mode. No effect, conversions results are correct. | D | ||
SDI | 8 | SDI is stuck low. Loss of SPI input communications to the device. Conversion data readout remains functional. | B |
SCLK | 9 | SCLK is stuck low. SPI communication is not possible. | B |
SDO/DRDY | 10 | SDO/DRDY is stuck low. SPI output communication is not possible. SPI input communication remains functional. The data-ready function with this pin is not functional. Device damage plausible if SDO/DRDY is shorted to ground for an extended period of time. | A |
DRDY | 11 | DRDY is stuck low, this pin is not monitored by the host. Normal operation. Device damage is plausible if DRDY is shorted to ground for an extended period of time. | A |
DRDY is stuck low, this pin is monitored by the host. No data-ready indication with DRDY to the host is possible. Device damage is plausible if DRDY is shorted to ground for an extended period of time. | A | ||
CLK | 12 | CLK is stuck low in external clock mode. The device is not functional. Conversion results are incorrect. | B |
CLK is stuck low in internal clock mode. No effect. Normal operation. | D | ||
IOVDD | 13 | The device is unpowered and not functional. | B |
DGND | 14 | No effect. Normal operation. | D |
CAPD | 15 | The device is partially unpowered and not functional. Device damage is plausible if CAPD is shorted to ground for an extended period of time. | A |
START | 16 | START is stuck low, this pin is in active use by the host. Loss of ability to control conversion timing. Conversion results are incorrect. | B |
START is stuck low, this pin is tied low in actual use (software control mode). No effect. Normal operation. | D | ||
AVSS | 17 | No effect. Normal operation. | D |
CAPA | 18 | The device is partially unpowered and is not functional. Device damage is plausible if CAPA is shorted to ground for an extended period of time. | A |
AVDD2 | 19 | The device is unpowered and not functional. | B |
AVDD1 | 20 | The device is unpowered and not functional. Observe that the absolute maximum ratings for the analog input and reference voltage pins of the device are met, otherwise device damage is plausible. | A |
Thermal pad | –- | No effect. Normal operation. | D |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
AINP | 1 | State of AINP is indeterminate. Conversion results are indeterminate. | B |
AINN | 2 | State of AINN is indeterminate. Conversion results are indeterminate. | B |
VCM | 3 | VCM output voltage is indeterminate. Conversion results are indeterminate. | B |
REFP | 4 | State of REFP is indeterminate. Conversion results are indeterminate. | B |
REFN | 5 | State of REFN is indeterminate. Conversion results indeterminate. | B |
RESET | 6 | RESET is stuck high. Loss of ability to reset the ADC with this pin. | B |
CS | 7 | State of CS is indeterminate. SPI communication is corrupted. | B |
SDI | 8 | State of SDI is indeterminate. Loss of SPI input communication to the device. Conversion data readout remains functional. | B |
SCLK | 9 | State of SCLK is indeterminate. SPI communication is corrupted. | B |
SDO/DRDY | 10 | State of SDO/DRDY is indeterminate. SPI output communication is not possible. SPI input communication remains functional. Loss of data-ready function from this pin. | B |
DRDY | 11 | DRDY is unconnected, this pin is not monitored by the host. No effect. Normal operation. | D |
DRDY is unconnected, this pin is monitored by the host. No data-ready indication with DRDY to the host is possible. | B | ||
CLK | 12 | CLK is open circuit in external clock mode. The device is not functional. Conversion results are incorrect. | B |
CLK is open circuit in internal clock mode. No effect. Normal operation. | D | ||
IOVDD | 13 | Device functionality is undetermined. The device is partially unpowered and not functional if the START digital input pin is held low. The device can be powered through the START digital input pin by an internal ESD diode conduction path to IOVDD. | B |
DGND | 14 | Device functionality is indeterminate. The device can be unpowered, or powered through digital inputs by an ESD diode path. | B |
CAPD | 15 | CAPD voltage is indeterminate. Conversion results are indeterminate. | B |
START | 16 | State of START is indeterminate. Conversion results are indeterminate. | B |
AVSS | 17 | Device functionality is indeterminate. The device is unpowered and not functional if the analog input or voltage reference pins are held low. The device can be powered through input or voltage reference drivers through an internal ESD diode conduction path. | B |
CAPA | 18 | CAPA voltage is indeterminate. Conversion results are indeterminate. | B |
AVDD2 | 19 | The device is partially unpowered and held in reset. The device is not functional. | B |
AVDD1 | 20 | Device functionality is indeterminate. The device is partially unpowered and not functional if the analog input or voltage reference pins are held low. The device can be powered through input or voltage reference drivers through an internal ESD diode conduction path. | B |
Thermal pad | — | The device remains functional with possible performance degradation. | C |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|---|
AINP | 1 | AINN | Conversion results are incorrect. Conversion result is close to 0 V. | B |
AINN | 2 | VCM | Conversion results are incorrect. | B |
VCM | 3 | REFP | Conversion results are incorrect. | B |
REFP | 4 | REFN | Conversion results are incorrect. | B |
REFN | 5 | RESET | Not considered. Corner pins. | D |
RESET | 6 | CS | Conversion results are incorrect. The device is not functional. | B |
CS | 7 | SDI | Loss of SPI input communication to the device if the driver source impedance of CS exceeds that of SDI. Loss of all SPI communication to the device if the driver source impedance of SDI exceeds that of CS. | B |
SDI | 8 | SCLK | Loss of SPI input communication to the device if the driver source impedance of SCLK exceeds that of SDI. Loss of all SPI communication to the device if the driver source impedance of SDI exceeds that of SCLK. | B |
SCLK | 9 | SDO/DRDY | Loss of SPI output communication from the device if the driver source impedance of SCLK exceeds that of SDO/DRDY. Loss of all SPI communication to the device if the driver source impedance of SDO/DRDY exceeds that of SCLK. Device damage is plausible if shorted together for an extended period of time. | A |
SDO/DRDY | 10 | DRDY | Not considered. Corner pins. | D |
DRDY | 11 | CLK | External clock mode. The device is not functional if the driver source impedance of DRDY exceeds that of CLK. Indeterminate state of DRDY if the driver source impedance of CLK exceeds that of DRDY. Device damage is plausible if shorted together for an extended period of time. | A |
Internal clock mode. The CLK pin has an external pullup or pulldown resistor to supply or ground (no active driver used). Normal operation. | D | |||
CLK | 12 | IOVDD | External clock mode. The device is not functional. Conversion results are incorrect. | B |
Internal clock mode. Normal operation. | D | |||
IOVDD | 13 | DGND | The device is partially unpowered and not functional. | B |
DGND | 14 | CAPD | The device is partially unpowered and not functional. Device damage is plausible if CAPD is shorted to ground for an extended period of time. | A |
CAPD | 15 | START | Not considered. Corner pins. | D |
START | 16 | AVSS | Conversion results are correct only if START is tied to DGND = AVSS in actual use. Otherwise, conversion results are not correct because of the inability to control conversions. | B |
AVSS | 17 | CAPA | The device is partially unpowered and not functional. | B |
CAPA | 18 | AVDD2 | CAPA is stuck high. Permanent device damage. | A |
AVDD2 | 19 | AVDD1 | No effect. Normal operation. | D |
AVDD1 | 20 | AINP | Not considered. Corner pins. | D |
Thermal pad | — | All pins | See the device pins short circuited to ground table (Table 4-6). | - |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
AINP | 1 | AINP is stuck high. Conversion results are correct only if AINP is tied to AVDD1 in actual use, otherwise conversion results are incorrect. | B |
AINN | 2 | AINN is stuck high. Conversion results are correct only if AINN is tied to AVDD1 in actual use, otherwise conversion results are incorrect. | B |
VCM | 3 | VCM is stuck high. Conversion results are incorrect. | B |
REFP | 4 | REFP is stuck high. Conversion results correct only if REFP is tied to AVDD1 in actual use, otherwise conversions results incorrect. | B |
REFN | 5 | REFN is stuck high. Conversion results are incorrect. | B |
RESET | 6 | RESET is stuck high. Normal operation except for the loss of RESET functionality. | B |
CS | 7 | CS is stuck high. SPI communication is not functional. | B |
SDI | 8 | SDI is stuck high. Loss of SPI input communication to the device. Conversion data readout remains functional. | B |
SCLK | 9 | SCLK is stuck high. SPI communication is not possible. | B |
SDO/DRDY | 10 | SDO/DRDY is stuck high. SPI communication is not functional. Data ready is not functional. Device damage is plausible if SDO/DRDY is shorted to the supply for an extended period of time. | A |
DRDY | 11 | DRDY is stuck high, this pin is not monitored. Normal operation. Device damage is plausible if DRDY is shorted to the supply for an extended period of time. | A |
DRDY is stuck high, this pin is monitored. No data-ready indication by DRDY to the host is possible. Device damage is plausible if DRDY is shorted to the supply for an extended period of time. | A | ||
CLK | 12 | CLK is stuck high in external clock mode. The device is not functional. Conversion results are incorrect. | B |
CLK is stuck high in internal clock mode. No effect. Normal operation. | D | ||
IOVDD | 13 | No effect. Normal operation. | D |
DGND | 14 | The device is not powered and not functional. | B |
CAPD | 15 | CAPD is stuck high. Permanent device damage. | A |
START | 16 | START is stuck high. Conversion results are correct only if START is tied to 5 V in actual use. Otherwise, conversion results are incorrect because of loss of ability to control conversions. | B |
AVSS | 17 | The device is unpowered and not functional. | B |
CAPA | 18 | CAPA is stuck high. Permanent device damage. | A |
AVDD2 | 19 | No effect. Normal operation. | D |
AVDD1 | 20 | No effect. Normal operation. | D |
Thermal pad | — | The device is unpowered and not functional. | B |