SDAA394 June 2026 LMG2650 , TLV431 , UCC25661
If the controller is giving LO pulses and then there is no pulse from the controller side and the controller is retrying after 1 sec, this is due to either the OCP fault or OLP fault. For OCP fault detection, the voltage across the ISNS pin and PGND has to be probed. If the peak voltage at the ISNS pin touches the threshold of 3.5V, it is the OCP fault. To avoid OCP fault, Risns must be reduced gradually, and TSET resistor divider must be adjusted accordingly by the design calculator to accommodate Pin vs VFBReplica graph within 2V-4V for no load to full load variation.
For OLP fault detection, FBReplica vs Pin graph has to be fitted one first prototype. The procedure to measure FBReplica in practical hardware is as follows:
Figure 1-2 FBReplica Measurement
Circuit
Figure 1-3 VFBReplica vs Pin GraphIf at any load, FBReplica touches 4.75V, then the fault at that load is OLP.