SDAA236 March 2026 DS90UB960-Q1
Between long and short packets, and between different long packets, the CSI-2 transmitter must enter low-power state (LPS). The transmitter is also required to transition from Low-Power to High-Speed signaling mode. During the LPS and time associated with the transition, the transmitter is idle and no data packets that can be sent, which means the CSI-2 output bandwidth is reduced.
The minimum CSI-2 High-Speed data transmission overhead consists of TLPX, THS-PREPARE, THS-ZERO, THS-SYNC, THS-TRAIL, and THS-EXIT as shown in Figure 3-3. The bandwidth is further reduced when operating in discontinuous CSI-2 Clock mode as it brings more CSI-2 overhead since data also cannot be sent while the clock lane is either in LP mode or transiting to HS mode, as shown in Figure 3-4.
Figure 3-4 Switching the Clock Lane
Between Clock Transmission and Low-Power Mode
Figure 3-5 High Speed Data Transmission
Burst