SCDA043 October   2022 MUX36D08 , TMUX6136 , TMUX6208 , TMUX6219 , TMUX6219-Q1 , TMUX6234 , TMUX6236 , TMUX7208 , TMUX7219 , TMUX7219-Q1 , TMUX7234 , TMUX7236 , TMUX7308F , TMUX7309F , TMUX7348F , TMUX7349F , TMUX8108 , TMUX8109 , TMUX8212

 

  1.   Abstract
  2.   Trademarks
  3. 1Differential, Single-Ended, and Common Mode Signals
  4. 2Characteristics of Interest for Selecting a Multiplexer for High Voltage Common Mode Applications
    1. 2.1 Operating Supply Range
    2. 2.2 Crosstalk and Bandwidth
    3. 2.3 Leakage Current
    4. 2.4 Fault Protection
  5. 3Multiplexers in High Voltage Common Mode Applications
    1. 3.1 PLC Multi-Channel Analog I/O Modules
    2. 3.2 CAN Bus Multiplexing Applications with High Voltage Common Mode
    3. 3.3 High Voltage Battery Cell Monitoring
  6. 4Recommended Multiplexers for High Voltage Common Mode Applications

PLC Multi-Channel Analog I/O Modules

Programmable logic controllers (PLCs) incorporate analog input or output modules that are implemented in fairly harsh factory automation environments and will routinely be exposed to high common mode voltages. A typical analog I/O module can incorporate a multiplexer being used in conjunction with an ADC. Usually, this type of use case has a single ADC that can use a multiplexer to switch between several different inputs as shown in
Figure 3-1.

Figure 3-1 PLC with Multiplexer Application

As seen above, the multiplexer can add much needed functionality to this application by expanding the amount of inputs the ADC can sample, however, the multiplexer also needs to be able to handle a potential common mode fault that can be introduced from the surrounding environment such as shown in Figure 3-2.

Figure 3-2 PLC with Common Mode Fault Event

The high common mode fault can shift the operating point of the application and the multiplexer must either have the supply capability to handle this shift, fault protection, or external components added to survive this event as illustrated in Figure 3-3.

Figure 3-3 PLC Analog I/O Common Mode Fault with Fault Protected or High Voltage Multiplexer