SBOU157 September 2015
The Source bar is beneath the top-level menu. It allows the user to select the input source, which can be from a live stream or a recorded stream. The Play and Stop buttons start and stop the streaming. The floppy disc icon starts a recording, which once stopped, will save the stream to a file. The progress bar shows playback progress, and at the end of the progress bar is the frame counter that shows the cumulative number of frames captured.
Figure 9. Source Bar