SBOU157 September 2015
Camera Profiles further lets users select from operating the ToF target in Short Range, Long Range, and No Calibration modes. The Long Range mode and Short Range mode differ in that the Long Range mode deploys the chipset’s de-aliasing feature to extend the range beyond the unambiguous distance. Please read Time-of-Flight Camera: An Introduction (SLOA190) for more information on de-aliasing and unambiguous distance. The purpose of the No Calibration selection is to enable one to compare and contrast the effect of calibration. New profiles can be created through the Edit Profiles option.