SBOU157 September 2015
Voxel Viewer is capable of connecting to multiple streams, but can only render one stream at a time. To connect a device to Voxel Viewer, simply plug in the ToF camera into the USB port. Only devices supported by the Voxel SDK will be detected and enumerated.
A compatible ToF camera can be connected after the Voxel Viewer is launched. If the Voxel Viewer is launched before the device is connected, the Voxel Viewer will display an inactive screen like the following image. From there, one can still connect a camera, just click the Refresh button to tell Voxel Viewer to rescan for attached ToF cameras.
Figure 17. Voxel Viewer Launched Without Connecting a Camera