SBOS854F March 2018 – June 2024
PRODUCTION DATA
The TMP1075 supports the SMBus Alert function. When the TMP1075 is operating in interrupt mode (TM = 1), the ALERT pin of the TMP1075 can be connected as an SMBus Alert signal. When a host senses that an alert condition is present on the ALERT line, the host sends an SMBus Alert command (00011001) on the bus. If the ALERT pin of the TMP1075 is active, the devices acknowledge the SMBus Alert command and respond by returning the device address on the SDA line. The eighth bit (LSB) of the device address byte indicates if the temperature exceeding THIGH or falling below TLOW caused the alert condition. This bit is equal to POL if the temperature is greater than or equal to THIGH. This bit is equal to POL if the temperature is less than TLOW. See Figure 7-8 for details of this sequence.
If multiple devices on the bus respond to the SMBus Alert command, arbitration during the device address portion of the SMBus Alert command determines which device clears the alert status. If the TMP1075 wins the arbitration, the ALERT pin becomes inactive at the completion of the SMBus Alert command. If the TMP1075 loses the arbitration, the ALERT pin remains active.