SBOK095 December   2024 TRF0208-SP

 

  1.   1
  2.    TRF0208-SP, Near-DC to 11GHz, Fully Differential RF Amplifier Single-Event Effects (SEE) Radiation Report
  3.   Trademarks
  4. Overview
  5. Single-Event Effects
  6. Test Device and Evaluation Board Information
  7. Irradiation Facility and Setup
  8. Depth, Range, and LETEFF Calculation
  9. Test Set-Up and Procedures
  10. Single-Event Latch-up (SEL) Results
  11. Single-Event Transients (SET) Results
  12. Event Rate Calculations
  13. 10Summary
  14.   A Total Ionizing Dose from SEE Experiments
  15.   B Confidence Interval Calculations
  16.   C References

Irradiation Facility and Setup

The heavy-ion species used for the SEE studies on this product were provided and delivered by the Texas A&M University (TAMU) Cyclotron Radiation Effects Facility [4], using a superconducting cyclotron and advanced electron cyclotron resonance (ECR) ion source. At the fluxes used, ion beams had good flux stability and high-irradiation uniformity over a 1-in diameter circular cross-sectional area for the in-air station. Uniformity is achieved by means of magnetic defocusing. The flux of the beam is regulated over a broad range spanning several orders of magnitude. For the bulk of these studies ion fluxes between 104 and 105 ions/cm2-s were used to provide a heavy-ion fluences between 106 and 107 ions/cm2.

For these experiments Holmium (165Ho), Silver (107Ag), Krypton (84Kr), Copper (63Cu) and Argon (40Ar) were used. Angles were used to increment the LETEFF, details are provided in Section 5. The 84Kr and 63Cu ions used had a total kinetic energy of 1259 and 944MeV in the vacuum, (15MeV/amu line) respectively. Ion beam uniformity for all tests was in the range of 88 to 97%.

Figure 4-1 shows the TRF0208-SP mounted on the EVM board in front of the beam exit port, as in the heavy-ion characterization. The beam port has a 1-mil Aramica (Kevlar®), 1in diameter to allow in-air testing while maintaining the vacuum in the accelerator with only minor ion energy losses. The air space between the device-under-test (DUT) and the beam exit port was set to 40 mm.

The data recorded in this report was based on finalized EVM boards with optimized component values that follow data sheet recommendations.

 TRF0208-SP Evaluation Board Mounted in Front of the Heavy-Ion Beam Exit PortFigure 4-1 TRF0208-SP Evaluation Board Mounted in Front of the Heavy-Ion Beam Exit Port