SBOK084 December   2023 SN54SC3T97-SEP , SN54SC3T98-SEP , SN54SC4T00-SEP , SN54SC4T02-SEP , SN54SC4T125-SEP , SN54SC4T32-SEP , SN54SC4T86-SEP

PRODUCTION DATA  

  1.   1
  2.   SN54SC4T125-SEP Single-Event Latch-Up (SEL) Radiation Report
  3.   Trademarks
  4. 1Overview
  5. 2Single-Event Effects (SEE)
  6. 3Test Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Results
    1. 5.1 SEL Results
    2. 5.2 Event Rate Calculations
  9. 6Summary
  10. 7References

SEL Results

During SEL characterization, the device was heated using forced hot air, maintaining IC temperature at 125°C. A FLIR (FLIR ONE Pro LT) thermal camera was used to validate die temperature to make sure that the device was accurately heated (see Figure 3-5). The species used for SEL testing was a Xenon (129Xe) ion at a linac energy of 25 MeV / µ with an angle-of-incidence of 0° for an LETEFF of 43 MeV-cm2 / mg. A fluence of approximately 1 × 107 ions/cm2 were used for the runs.

The three devices were powered up and exposed to the heavy-ions using the maximum recommended supply voltage of 5.5-V using a National Instruments PXI Chassis PXIe-1085. The run duration to achieve this fluence was approximately 2 minutes. As listed in Table 5-1, no SEL events were observed during the nine runs, indicating that the SN54SC4T125-SEP is SEL-free. Figure 5-1, Figure 5-2, and Figure 5-3 show the plot of current versus time for run numbers one, four, and seven, respectively.

Table 5-1 Summary of SN54SC4T125-SEP Test Conditions and Results
Run NumberUnit NumberDistance (mm)Temperature
(°C)
IonAngleFLUX
(ions × cm2 / mg)
Fluence
(number of ions)
LETEFF
(MeV × cm2/ mg)
Did a SEL event occur?
1170123Xe0°1.00E+051.00E+0743No
2170123Xe0°1.00E+051.00E+0743No
3170123Xe0°1.00E+051.00E+0743No
4270123Xe0°1.00E+051.00E+0743No
5270123Xe0°1.00E+051.00E+0743No
6270123Xe0°1.00E+051.00E+0743No
7370122Xe0°1.00E+051.00E+0743No
8370122Xe0°1.00E+051.00E+0743No
9370122Xe0°1.00E+051.00E+0743No
GUID-20231004-SS0I-GQ4C-4CPQ-2MM20QBWGZNH-low.pngFigure 5-1 Current versus Time for Run Number 1 of the SN54SC4T125-SEP at T = 125°C
GUID-20231004-SS0I-PWT2-CQJC-PFWFTZNXGXFM-low.pngFigure 5-2 Current versus Time for Run Number 4 of the SN54SC4T125-SEP at T = 125°C
GUID-20231004-SS0I-3FD6-CDDH-CKF6WM61JWT8-low.pngFigure 5-3 Current versus Time for Run 7 of the SN54SC4T125-SEP at T = 125°C

No SEL events were observed, indicating that the SN54SC4T125-SEP is SEL-immune at LETEFF = 43 MeV-cm2 / mg and T = 125°C. Using the MFTF method shown in Single-Event Effects (SEE) Confidence Interval Calculations, the upper-bound cross-section (using a 95% confidence level) is calculated as:

Equation 1. σSEL ≤ 1.23 × 10–7 cm2 / device for LETEFF = 43 MeV-cm2 / mg and T = 125°C