SBOK078 October 2023 SN54SC4T08-SEP
PRODUCTION DATA
The heavy ion species used for the SEE studies on this product were provide and delivered by the Facility for Rare Isotope Beams (FRIB) at Michigan State University – FRIB Single Event Effects (FSEE) Facility’s linear accelerator. The FSEE Facility has a dedicated beamline built on the FRIB linac infrastructure with a user experimental station at the end of the FSEE beamline. Ion beams are delivered with high uniformity over a 1-inch diameter exposure area using a thin vacuum window. For this study, ion flux of 105 ions/s-cm2 was used to provide heavy ion fluence of 1 × 107 ions / cm2 using 129Xe ion at a linac energy of 25 MeV/µ. Ion beam non-uniformity for all tests was between 5.1% to 6.7%.
Figure 4-1 shows one of the three SN54SC4T08-SEP test board used for experiments at the MSU FSEE facility. The in-air gap between the device and the ion beam port window was maintained at 70 mm for all runs.
Figure 4-1 SN54SC4T08-SEP Evaluation
Board at the MSU FSEE Facility