SBOK070 November   2022 OPA4H199-SEP

 

  1.   OPA4H199-SEP Single-Event Latch-Up (SEL) Radiation Report
  2.   Trademarks
  3. 1Overview
  4. 2SEE Mechanisms
  5. 3Test Device and Test Board Information
  6. 4Irradiation Facility and Setup
  7. 5Results
    1. 5.1 SEL Results
  8. 6Summary
  9.   A Confidence Interval Calculations
  10.   B References

Confidence Interval Calculations

For conventional products where hundreds of failures are seen during a single exposure, one can determine the average failure rate of parts being tested in a heavy-ion beam as a function of fluence with high degree of certainty and reasonably tight standard deviation, and thus have a good deal of confidence that the calculated cross-section is accurate.

With radiation-hardened parts however, it is difficult to determine the cross-section because often few or no failures are observed during an entire exposure. Determining the cross-section using an average failure rate with standard deviation is no longer a viable option, and the common practice of assuming a single error occurred at the conclusion of a null-result can end up in a greatly underestimated cross-section.

In cases where observed failures are rare or non-existent, the use of confidence intervals and the chi-squared distribution is indicated. The chi-squared distribution is particularly well-suited for the determination of a reliability level when the failures occur at a constant rate. In the case of SEE testing where the ion events are random in time and position within the irradiation area, one expects a failure rate that is independent of time (presuming that parametric shifts induced by the total ionizing dose do not affect the failure rate), and thus the use of chi-squared statistical techniques is valid (because events are rare, an exponential or Poisson distribution is usually used).

In a typical SEE experiment, the device-under-test (DUT) is exposed to a known, fixed fluence (ions/cm2) while the DUT is monitored for failures. This is analogous to fixed-time reliability testing and, more specifically, time-terminated testing where the reliability test is terminated after a fixed amount of time whether or not a failure has occurred (in the case of SEE tests fluence is substituted for time and hence it is a fixed fluence test [5]). Calculating a confidence interval specifically provides a range of values which is likely to contain the parameter of interest (the actual number of failures/fluence). Confidence intervals are constructed at a specific confidence level. For example, a 95% confidence level implies that if a given number of units were sampled numerous times and a confidence interval estimated for each test, the resulting set of confidence intervals would bracket the true population parameter in about 95% of the cases.

To estimate the cross-section from a null-result (no fails observed for a given fluence) with a confidence interval, we start with the standard reliability determination of lower-bound (minimum) mean-time-to-failure for fixed-time testing (an exponential distribution is assumed) in Equation 2:

Equation 2. MTTF=2nTχ2(d+1);100(1-α2)2

Where:

  • MTTF is the minimum (lower-bound) mean-time-to-failure,

  • n is the number of units tested (presuming each unit is tested under identical conditions),

  • T is the test time,

  • and χ2 is the chi-square distribution evaluated at 100(1 – α / 2) confidence level

  • d is the degrees-of-freedom (the number of failures observed).

With slight modification for our purposes we invert the inequality and substitute F (fluence) in the place of T as shown in Equation 3:

Equation 3. MFTF=2nFχ2(d+1);100(1-α2)2

Where:

  • MFTF is mean-fluence-to-failure

  • F is the test fluence

  • Χ2 is the chi-square distribution evaluated at 100(1 – α / 2) confidence

  • d is the degrees-of-freedom (the number of failures observed).

The inverse relation between MTTF and failure rate is mirrored with the MFTF. Thus the upper-bound cross-section is obtained by inverting the MFTF as shown in Equation 4:

Equation 4. σ=χ2(d+1);100(1-α2)22nF

Assume that all tests are terminated at a total fluence of 106 ions/cm2. Also assume there are a number of devices with very different performances that are tested under identical conditions. Assume a 95% confidence level (σ = 0.05). Note that as d increases from 0 events to 100 events, the actual confidence interval becomes smaller, indicating that the range of values of the true value of the population parameter (in this case the cross-section) is approaching the mean value + 1 standard deviation. This makes sense when one considers that as more events are observed the statistics are improved such that uncertainty in the actual device performance is reduced.

Table A-1 Experimental Example Calculation of MFTF and σ Using a 95% Confidence Interval(1)
Degrees-of-Freedom (d)2(d + 1)χ2 @ 95%Calculated Cross-Section (cm2)
Upper-Bound @ 95% ConfidenceMeanAverage + Standard Deviation
027.383.69E–060.00E+000.00E+00
1411.145.57E–061.00E–062.00E–06
2614.457.22E–062.00E–063.41E–06
3817.538.77E–063.00E–064.73E–06
41020.481.02E–054.00E–066.00E–06
51223.341.17E–055.00E–067.24E–06
102236.781.84E–051.00E–051.32E–05
50102131.846.59E–055.00E–055.71E–05
100202243.251.22E–041.00E–041.10E–04
Using a 95% confidence interval for several different observed results (d = 0, 1, 2,…100 observed events during fixed-fluence tests) assuming 106 ions/cm2 for each test. Note that as the number of observed events increases the confidence interval approaches the mean.