SBOK070 November   2022 OPA4H199-SEP

 

  1.   OPA4H199-SEP Single-Event Latch-Up (SEL) Radiation Report
  2.   Trademarks
  3. 1Overview
  4. 2SEE Mechanisms
  5. 3Test Device and Test Board Information
  6. 4Irradiation Facility and Setup
  7. 5Results
    1. 5.1 SEL Results
  8. 6Summary
  9.   A Confidence Interval Calculations
  10.   B References

Irradiation Facility and Setup

The heavy ion species used for the SEE studies on this product were provided and delivered by the TAMU Cyclotron Radiation Effects Facility [3] using a superconducting cyclotron and advanced electron cyclotron resonance (ECR) ion source. Ion beams are delivered with high uniformity over a 1-inch diameter circular cross sectional area for the in-air station. Uniformity is achieved by means of magnetic defocusing. The intensity of the beam is regulated over a broad range spanning several orders of magnitude. For the bulk of these studies, ion fluxes between 104 and 105 ions/s-cm2 were used to provide heavy ion fluences between 106 and 107 ions/cm2. For these experiments Silver (Ag) ions were used. Ion beam uniformity for all tests was in the range of 91% to 98%.