SBOA551 June   2022 INA240

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2One, Versus Two Reference Pins
  5. 3Bidirectional Current Sense Amplifier Topologies
    1. 3.1 Single-Stage Difference Amplifier
    2. 3.2 Difference Amplifier Input Followed by Noninverting Output Buffer
    3. 3.3 Voltage Feedback Multi-Stage Difference Amplifier
    4. 3.4 Single-Stage Current Feedback
    5. 3.5 Current Feedback Multi-Stage Difference Amplifier
    6. 3.6 Isolated Bidirectional Current Sensors
  6. 4Options for Driving Reference Pins and Input Referred Reference Error
  7. 5Resistor Divider as Reference
    1. 5.1 Resistor Divider and Equivalent Circuit
    2. 5.2 Reference Source Impedance Error in Difference Amplifier
    3. 5.3 Reference Source Impedance Error in Voltage Feedback Multi-Stage CSA
    4. 5.4 Reference Source Impedance Error in Current Feedback Multi-Stage CSA
    5. 5.5 Reference Source Impedance Error in Difference Amplifier with Output Buffer
  8. 6Examples
    1. 6.1 Calculating Reference Source Impedance Error in Difference Amplifier
    2. 6.2 Calculating Reference Source Impedance Error in Voltage Feedback Multi-Stage CSA
    3. 6.3 Calculating Reference Source Impedance Error in Current Feedback Multi-Stage CSA
  9. 7Summary

Options for Driving Reference Pins and Input Referred Reference Error

Three methods are commonly used to drive the reference pin, namely with a reference voltage IC, with a supply divider, or with a supply divider followed by a buffer. These options are illustrated in Figure 4-1.

Figure 4-1 Options Driving Reference Pin

Each of these has its own pros and cons. A high-level comparison is show in Table 4-1.

Table 4-1 Comparison of Reference-setting Methods
Reference Source Accuracy Power Dissipation Cost
Reference IC High Low High
Divider Low High Low
Divider + buffer Medium Medium Medium

From a performance perspective, a reference IC is the best choice. The electrical characteristics of a reference are well defined and production tested. Key parameters such as offset, drift, and noise are excellent. Such reference provides a stable, clean output voltage that is ideal for data acquisition. Sometimes a reference already exists because it is required by other components such as ADC. It might be possible to use the existing reference without incurring additional cost.

The most affordable reference is the supply divider, where the reference voltage is derived from the device power supply with a resistor divider. Any value in between 0 V and supply is possible. It is a natural tendency to use large resistors so that power dissipation is kept to a minimum. However, a large divider adds to the internal resistor of the reference pin and breaks the balance of the resistor network. To reduce such impact, The Thevenin's equivalent resistance should be kept as small as possible. But it may become impractical if the resistance values get too low and consequently the power dissipation becomes too great. In theory, an ideal point between the two extremes is possible, which may be suitable for certain applications. The following sections look deeper into the performance impact of such dividers. Another aspect that should not be ignored is the quality of the power supply itself.

For applications that are power sensitive, the third approach might be a good option. A large resistor divider followed by a general-purpose buffer can provide a good reference at a reasonable cost. The buffer isolates the divider from the internal resistor network and provides a virtual ground for the reference pin. The buffer amplifier does not have to be high performance. Because its non-idealities are added to the CSA output, they get divided down by the CSA gain when referred to input. Figure 4-2 illustrates the idea of referring reference error to equivalent input error.

Regardless of the method chosen, in reality there is going to be some error introduced by the reference source. It may be necessary to account for this error if it is not negligible. To do this, it is important to keep the calculation consistent with that for the rest of the error sources. In other words, either input referred or output referred calculation can be used. But the two methods should not be mixed.

Figure 4-2 Refer Reference Voltage Error to Device Input

Reference source errors are directly added to the output. To compare or combine with other error sources, the reference errors are normally referred to input. As an example, the external reference source in Figure 4-2(a) has an offset Vos_x in addition to its ideal value of Vref_x. when calculating input referred error contribution, Vos_x needs to be divided by the CSA gain. Figure 4-2(b) shows the equivalent circuit after Vos_x is referred to input.

Even though offset of the reference source is used as an example, the same principle applies to other non-idealities, including gain error, temperature drift, and noise, to name a few.