- Connect the ADC3910D125EVM to the TSWDC155EVMEVM
through the FMC connector.
- Connect the FTDI dongle to the ADC3910D125EVM via
J2 of the ADC3910D125EVM.
- Connect the JTAG dongle provided with the
TSWDC155EVMEVM onto the JTAG Connector of the
TSWDC155EVM.
- Make sure Jumper J2 on TSWDC155EVM is connected
between pins one and two.
- Connect a +12V power supply to the DC Barrel Jack
connector of the ADC3910D125EVM using the included
power supply cable.
- Connect a mini USB cable from the PC to the FTDI
dongle installed on the ADC3910D125EVM.
- Connect a USB C cable from the PC to the USB C
connector on the TSWDC155EVM.
- Connect a micro USB cable from the PC to the JTAG
dongle connected to the TSWDC155EVM
- Connect a bandpass filtered clock signal source
to J7 labeled CLK of the ADC3910D125EVM.
- Connect a bandpass filtered analog input source
to J8 and/or J10 of the ADC3910D125EVM labeled
INAp and INBp, respectively.
If all the steps above were followed correctly,
then the final setup looks like the following: