SBAU227A March   2014  – June 2021

 

  1.   Trademarks
  2. 1Introduction
  3. 2Performance Specification Summary
  4. 3Modifications
    1. 3.1 Output Voltage Set Point
    2. 3.2 Output Voltage Set Point Using I2C Interface
      1. 3.2.1 PC Preparation
      2. 3.2.2 Connect the PC
      3. 3.2.3 Voltage Scaling Procedure
    3. 3.3 Output Filter and Closed Loop Response
  5. 4Test Setup and Results
    1. 4.1 Input/Output Connections
    2. 4.2 Start Up Procedure
    3. 4.3 Efficiency
    4. 4.4 Load Regulation
    5. 4.5 Line Regulation
    6. 4.6 Load Transient Response
    7. 4.7 Output Voltage Ripple
    8. 4.8 Start Up
    9. 4.9 Shut Down
  6. 5Board Layout
    1. 5.1 Board Layout
  7. 6Schematic, Bill of Materials and Reference
    1. 6.1 Schematic
    2. 6.2 Bill of Materials
    3. 6.3 Reference
  8. 7Revision History

Voltage Scaling Procedure

Set voltage scaling by using the following steps:

  1. Go to Program Files and click on the TPS56X20 I2C TEST PANEL Application. The TPS56X20 I2C TEST PANEL will load as shown in Figure 3-2.
    GUID-081E004F-7AFB-46A3-BCE3-FDEE601EDE0E-low.pngFigure 3-2 TPS56X20 I2C TEST PANEL
  2. As a first step before sending a VOUT command, click the write command On the EXT Power Settings block as shown in Figure 3-3.
    GUID-18EEC3C7-A910-4B2C-A4E6-8FDEB3DF1672-low.pngFigure 3-3 EXT Power Settings
  3. Go to the VOUTS control block and click on the ALL VOUTS control, illustrated in Figure 3-4. The drop down menu gives an option to select different VOUT.
    GUID-0FBDBC4F-BAC2-4EDB-BE28-5A5DE6350F37-low.pngFigure 3-4 ALL VOUTS Control
  4. Select a particular value and click on WRITE VOUT switch.

Observe that the Voltage at TP6 relative to TP7 is changed to the programmed VOUT value.