SBAA634 April 2026 TAA5212 , TAA5412-Q1 , TAC5111 , TAC5111-Q1 , TAC5112 , TAC5112-Q1 , TAC5211 , TAC5212 , TAC5311-Q1 , TAC5312-Q1 , TAC5412-Q1 , TAD5112 , TAD5112-Q1 , TAD5212 , TAD5212-Q1
The TAx5x1x/TAx5x1x-Q1 family of devices include dual-channel, high-performance, analog to-digital converters for audio applications. This family of devices supports highly configurable inputs to allow the device to achieve high performance even in the presence of large common-mode signals.
Common Mode Rejection Ratio (CMRR) is an important specification in determining the performance of an audio ADC when it is placed in systems that can contain common-mode interferences on the signal lines. One example of such must be the 50-60Hz supply line interference. This application note describes how to configure the input common-mode level tolerance on the TAC5x1x/TAC5x1x-Q1 devices, along with the impact on certain performance parameters such as SNR, THD+N, and so on.
This application note is applicable for the following devices in the family: