ZHCSQ69B june 2022 – august 2023 TPS7A15
PRODUCTION DATA
The load-step transient response is the output voltage response by the LDO to a step in load current while output voltage regulation is maintained. See the Typical Characteristics section for the typical load transient response. There are two key transitions during a load transient response: the transition from a light to a heavy load, and the transition from a heavy to a light load. The regions in Load Transient Waveform are broken down as described in this section. Regions A, E, and H are where the output voltage is in steady-state operation.
During transitions from a light load to a heavy load, the following behavior can be observed:
During transitions from a heavy load to a light load, the:
A larger output capacitance reduces the peaks during a load transient but slows down the response time of the device. A larger dc load also reduces the peaks because the amplitude of the transition is lowered and a higher current discharge path is provided for the output capacitor.