SLUS791A July   2007  – September 2015 TPS28226

PRODUCTION DATA.  

  1. 1 Features
  2. 2 Applications
  3. 3 Description
  4. 4 Revision History
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
    6. 6.6 Switching Characteristics
    7. 6.7 Typical Characteristics
  7. 7 Detailed Description
    1. 7.1 Overview
    2. 7.2 Functional Block Diagram
    3. 7.3 Feature Description
      1. 7.3.1 Undervoltage Lockout (UVLO)
      2. 7.3.2 Output Active Low
      3. 7.3.3 Enable/Power Good
      4. 7.3.4 3-State Input
        1. 7.3.4.1 TPS28226 3-State Exit Mode
        2. 7.3.4.2 External Resistor Interference
      5. 7.3.5 Bootstrap Diode
      6. 7.3.6 Upper and Lower Gate Drivers
      7. 7.3.7 Dead-Time Control
      8. 7.3.8 Thermal Shutdown
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
        1. 8.2.2.1 Four Phases Driven by TPS28226 Driver
        2. 8.2.2.2 Switching The MOSFETs
        3. 8.2.2.3 List of Materials
      3. 8.2.3 Application Curves
    3. 8.3 System Examples
  9. 9 Power Supply Recommendations
  10. 10Layout
    1. 10.1 Layout Guidelines
    2. 10.2 Layout Example
  11. 11Device and Documentation Support
    1. 11.1 Device Support
      1. 11.1.1 Third-Party Products Disclaimer
    2. 11.2 Documentation Support
      1. 11.2.1 Related Documentation
    3. 11.3 Community Resources
    4. 11.4 Trademarks
    5. 11.5 Electrostatic Discharge Caution
    6. 11.6 Glossary
  12. 12Mechanical, Packaging, and Orderable Information

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

8 Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

8.1 Application Information

To effect fast switching of power devices and reduce associated switching power losses, a powerful MOSFET driver is employed between the PWM output of controllers and the gates of the power semiconductor devices. Also, MOSFET drivers are indispensable when it is impossible for the PWM controller to directly drive the MOSFETs of the switching devices. With the advent of digital power, this situation will be often encountered because the PWM signal from the digital controller is often a 3.3-V logic signal which cannot effectively turn on a power switch. Level shifting circuitry is needed to boost the 3.3-V signal to the gate-drive voltage (such as 12 V) in order to fully turn on the power device and minimize conduction losses. Traditional buffer drive circuits based on NPN/PNP bipolar transistors in totem-pole arrangement, being emitter follower configurations, prove inadequate with digital power because they lack level-shifting capability. MOSFET drivers effectively combine both the level-shifting and buffer-drive functions.

MOSFET drivers also find other needs such as minimizing the effect of high-frequency switching noise by locating the high-current driver physically close to the power switch, driving gate-drive transformers and controlling floating power-device gates, reducing power dissipation and thermal stress in controllers by moving gate charge power losses from the controller into the driver.

8.2 Typical Application

The DC-DC converter in Figure 25 displays the schematic of the TPS28226 in a multiphase high-current step-down power supply (only one phase is shown). This design uses a single high-side MOSFET Q10 and two low-side MOSFETs Q8 and Q9, the latter connected in parallel. The TPS28226 is controlled by multiphase buck DC-to-DC controller like TPS40090. As TPS28226 has internal shoot-through protection only one PWM control signal is required for each channel.

TPS28226 fig25b_lus710.gif Figure 25. One of Four Phases Driven by TPS28226 Driver in 4-Phase VRM Reference Design

8.2.1 Design Requirements

The VRM Reference Design is capable of driving 35 A per phase. In this example it has a nominal input voltage of 12 V within a tolerance range of ±5%. The switching frequency is 500 kHz. The nominal duty cycle is 10%, therefore the low-side MOSFETs are conducting 90% of the time. By choosing lower RDS(on) the conduction losses of the switching elements are minimized.

Table 2. VRM Reference Design Requirements

DESIGN PARAMETER VALUE
Supply voltage 12 V ±5%
Output voltage 0.83 V to 1.6 V
Frequency 500 kHz
Peak-to-peak output voltage variation on load current transient (0 A to 100 A ) within 1 µs <160 mV
Dynamic output voltage change slew rate 12.25 mV per 5 µs

8.2.2 Detailed Design Procedure

The bootstrap current can be limited by changing R32 to prevent overcharging of the bootstrap capacitor and to slow the turn-on transition of the high-side MOSFET. This reduces the peak amplitude and ringing of the switching node. Furthermore it minimizes the possibility of Cdv/dt-induced shoot-through of the low-side MOSFETs. The snubbers composed of C50 with R51 and C51 with R52 help to reduce switching noise.

The output component selection considers the requirement of a fast transient response. For output capacitors small capacitance values are chosen because of rapid changes of the output voltage. These changes also require an inductor with low inductance. Due to the small duty cycle the low-side MOSFETs conduct a long time. Two low-side MOSFETs are selected to increase both thermal performance and efficiency.

8.2.2.1 Four Phases Driven by TPS28226 Driver

When using the same power stage Figure 25, the driver with the optimal drive voltage and optimal dead time can boost efficiency up to 5%. The optimal 8-V drive voltage versus 5-V drive contributes 2% to 3% efficiency increase and the remaining 1% to 2% can be attributed to the reduced dead time. The 7-V to 8-V drive voltage is optimal for operation at switching frequency range above 400 kHz and can be illustrated by observing typical RDS(on) curves of modern FETs as a function of their gate-drive voltage. This is shown in Figure 26.

Figure 26 and Figure 27 show that the RDS(on) at 5-V drive is substantially larger than at 7 V and above that the RDS(on) curve is almost flat. This means that moving from 5-V drive to an 8-V drive boosts the efficiency because of lower RDS(on) of the MOSFETs at 8 V. Further increase of drive voltage from 8 V to 12 V only slightly decreases the conduction losses but the power dissipated inside the driver increases dramatically (by 125%). The power dissipated by the driver with 5-V, 8-V and 12-V drive as a function of switching frequency from 400 kHz to 800 kHz. It should be noted that the 12-V driver exceeds the maximum dissipated power allowed for an SOIC-8 package even at 400-kHz switching frequency.

TPS28226 fig31_lus710.gif
Figure 26. RDS(on) of MOSFET as Function of VGS
TPS28226 wave30_lus710.gif
Figure 27. Drive Power as Function of VGS and FSW

8.2.2.2 Switching The MOSFETs

Driving the MOSFETs efficiently at high switching frequencies requires special attention to layout and the reduction of parasitic inductances. Efforts need to be done both at the driver’s die and package level and at the PCB layout level to keep the parasitic inductances as low as possible. Figure 28 shows the main parasitic inductances and current flow during turning ON and OFF of the MOSFET by charging its CGS gate capacitance.

TPS28226 fig22_lus710.gif Figure 28. MOSFET Drive Paths and Main Circuit Parasitics

The ISOURCE current charges the gate capacitor and the ISINK current discharges it. The rise and fall time of voltage across the gate defines how quickly the MOSFET can be switched. The timing parameters specified in datasheet for both upper and lower driver are shown in Figure 16 and Figure 17 where 3-nF load capacitor has been used for the characterization data. Based on these actual measurements, the analytical curves in Figure 29 and Figure 30 show the output voltage and current of upper and low side drivers during the discharging of load capacitor. The left waveforms show the voltage and current as a function of time, while the right waveforms show the relation between the voltage and current during fast switching. These waveforms show the actual switching process and its limitations because of parasitic inductances. The static VOUT/ IOUT curves shown in many datasheets and specifications for the MOSFET drivers do not replicate actual switching condition and provide limited information for the user.

Turning Off of the MOSFET needs to be done as fast as possible to reduce switching losses. For this reason the TPS28226 driver has very low output impedance specified as 0.4 Ω typical for lower driver and 1 Ω typical for upper driver at DC current. Assuming 8-V drive voltage and no parasitic inductances, one can expect an initial sink current amplitude of 20 A and 8 A respectively for the lower and upper drivers. With pure R-C discharge circuit for the gate capacitor, the voltage and current waveforms are expected to be exponential. However, because of parasitic inductances, the actual waveforms have some ringing and the peak current for the lower driver is about 4 A and about 2.5 A for the upper driver (Figure 29 and Figure 30). The overall parasitic inductance for the lower drive path is estimated as 4 nH and for the upper drive path as 6 nH. The internal parasitic inductance of the driver, which includes inductances of bonded wires and package leads, can be estimated for SOIC-8 package as 2 nH for lower gate and 4 nH for the upper gate. Use of DFN-8 package reduces the internal parasitic inductances by approximately 50%.

TPS28226 fig23_lus710.gif Figure 29. LGATE Turning Off Voltage and Sink Current vs Time (Related Switching Diagram (right))
TPS28226 fig24_lus710.gif Figure 30. UGATE Turning Off Voltage and Sink Current vs Time (Related Switching Diagram (right))

8.2.2.3 List of Materials

For this specific example see Table 3. The component vendors are not limited to those shown in the table below. It should be noted that in this example, the power MOSFET packages were chosen with drains on top. The decoupling capacitors C47, C48, C65, and C66 were chosen to have low profiles. This allows the designer to meet good layout rules and place a heatsink on top of the FETs using an electrically isolated and thermally conductive pad.

Table 3. List of Materials

REF DES COUNT DESCRIPTION MANUFACTURE PART NUMBER
C47, C48, C65, C66 4 Capacitor, ceramic, 4.7 μF, 16 V, X5R 10%, low profile 0.95 mm, 1206 TDK C3216X5R1C475K
C41, C42 2 Capacitor, ceramic, 10 μF, 16 V, X7R 10%, 1206 TDK C3216X7R1C106K
C50, C51 2 Capacitor, ceramic, 1000 pF, 50 V, X7R, 10%, 0603 Std Std
C23 1 Capacitor, ceramic, 0.22 μF, 16 V, X7R, 10%, 0603 Std Std
C25, C49, C71 3 Capacitor, ceramic, 1 μF, 16 V, X7R, 10%, '0603 Std Std
L3 1 Inductor, SMT, 0.12 μH, 31 A, 0.36 mΩ, 0.400 x 0.276 Pulse PA0511-101
Q8, Q9 2 Mosfet, N-channel, VDS 30 V, RDS 2.4 mΩ, ID 45 A, LFPAK-i Renesas RJK0301DPB-I
Q10 1 Mosfet, N-channel, VDS 30 V, RDS 6.2 mΩ, ID 30 A, LFPAK-i Renesas RJK0305DPB-I
R32 1 Resistor, chip, 0 Ω, 1/10 W, 1%, '0805 Std Std
R51, R52 2 Resistor, chip, 2.2 Ω, 1/10 W, 1%, '0805 Std Std
U7 1 Device, High Frequency 4-A Sink Synchronous Buck MOSFET Driver, DFN-8 Texas Instruments TPS28226DRB

8.2.3 Application Curves

Efficiency achieved using TPS28226 driver with 8-V drive at different switching frequencies a similar industry 5-V driver using the power stage in Figure 25 is shown in Figure 31, Figure 32, Figure 33, Figure 34 and Figure 35.

TPS28226 wave28d_lus710.gif
Figure 31. Efficiency vs Load Current
TPS28226 wave28a_lus710.gif
Figure 33. Efficiency vs Load Current
TPS28226 wave28b_lus710.gif
Figure 35. Efficiency vs Load Current
TPS28226 wave28e_lus710.gif
Figure 32. Efficiency vs Load Current
TPS28226 wave28c_lus710.gif
Figure 34. Efficiency vs Load Current

8.3 System Examples

Figure 36, Figure 37 and Figure 38 below illustrate typical implementations of the TPS28226 in step-down power supplies.

TPS28226 alt_lus791.gif Figure 36. One-Phase POL Regulator
TPS28226 typapp2_lus791.gif Figure 37. Driver for Synchronous Rectification with Complementary Driven MOSFETs
TPS28226 typapp3_lus791.gif Figure 38. Multi-Phase Synchronous Buck Converter