ZHCSK56A August 2019 – July 2020 TMUX1208-Q1
PRODUCTION DATA
The TMUX1208-Q1 has a transmission-gate topology. Any mismatch in capacitance between the NMOS and PMOS transistors results in a charge injected into the drain or source during the falling or rising edge of the gate signal. The amount of charge injected into the source or drain of the device is known as charge injection, and is denoted by the symbol QC. Figure 7-7 shows the setup used to measure charge injection from source (Sx) to drain (D).
Figure 7-7 Charge-Injection Measurement Setup