ZHCSMN3B February 2021 – January 2023 OPA855-Q1
PRODUCTION DATA
Figure 12-1 Layout RecommendationWhen configuring the OPA855-Q1 as a transimpedance amplifier additional care must be taken to minimize the inductance between the avalanche photodiode (APD) and the amplifier. Always place the photodiode on the same side of the PCB as the amplifier. Placing the amplifier and the APD on opposite sides of the PCB increases the parasitic effects due to via inductance. APD packaging can be quite large which often requires the APD to be placed further away from the amplifier than ideal. The added distance between the two device results in increased inductance between the APD and op amp feedback network as shown in Figure 12-2. The added inductance is detrimental to a decompensated amplifiers stability since it isolates the APD capacitance from the noise gain transfer function. The noise gain is given by Equation 3. The added PCB trace inductance between the feedback network increases the denominator in Equation 3 thereby reducing the noise gain and the phase margin. In cases where a leaded APD in a TO can is used inductance should be further minimized by cutting the leads of the TO can as short as possible.
The layout shown in Figure 12-2 can be improved by following some of the guidelines shown in Figure 12-3. The two key rules to follow are:
where
Figure 12-2 Non-Ideal
TIA Layout
Figure 12-3 Improved
TIA Layout