ZHCSDQ7 May   2015 HD3SS3212

PRODUCTION DATA.  

  1. 1 特性
  2. 2 应用
  3. 3 说明
  4. 4 简化电路原理图
  5. 5 修订历史记录
  6. 6 Device Comparison Table
  7. 7 Pin Configuration and Functions
  8. 8 Specifications
    1. 8.1 Absolute Maximum Ratings
    2. 8.2 ESD Ratings
    3. 8.3 Recommended Operating Conditions
    4. 8.4 Thermal Information
    5. 8.5 Electrical Characteristics
    6. 8.6 High-Speed Performance Parameters
    7. 8.7 Switching Characteristics
  9. 9 Parameter Measurement Information
  10. 10Detailed Description
    1. 10.1 Overview
    2. 10.2 Functional Block Diagram
    3. 10.3 Feature Description
      1. 10.3.1 Output Enable and Power Savings
    4. 10.4 Device Functional Modes
  11. 11Application and Implementation
    1. 11.1 Application Information
    2. 11.2 Typical Applications
      1. 11.2.1 Down Facing Port for USB3.1 Type C
        1. 11.2.1.1 Design Requirements
        2. 11.2.1.2 Detailed Design Procedure
        3. 11.2.1.3 Application Curves
      2. 11.2.2 Up Facing Port for USB3.1 Type C
      3. 11.2.3 PCIE/SATA/USB
      4. 11.2.4 PCIE/eSATA
      5. 11.2.5 USB/eSATA
      6. 11.2.6 MIPI Camera Serial Interface
  12. 12Power Supply Recommendations
  13. 13Layout
    1. 13.1 Layout Guidelines
    2. 13.2 Layout Example
  14. 14器件和文档支持
    1. 14.1 相关链接
    2. 14.2 社区资源
    3. 14.3 商标
    4. 14.4 静电放电警告
    5. 14.5 术语表
  15. 15机械、封装和可订购信息

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

11 Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

11.1 Application Information

The HD3SS3212 is a generic 2-channel high-speed mux/demux type of switch that can be used for routing high-speed signals between two different locations on a circuit board. The HD3SS3212 supports several high-speed data protocols with a differential amplitude of <1800 mVpp and a common mode voltage of <2.0 V, as with USB 3.0 and DisplayPort 1.2. The device’s one select input (SEL) pin can easily be controlled by an available GPIO pin within a system or from a microcontroller.

The HD3SS3212 with its adaptive common mode tracking technology can support applications where the common mode is different between the RX and TX pair. The two USB3.1 Type C connector applications show both a host and device side. The cable between the two connectors swivels the pairs to properly route the signals to the correct pin. The other applications are more generic because different connectors can be used.

Many interfaces require AC coupling between the transmitter and receiver. The 0402 capacitors are the preferred option to provide AC coupling; 0603 size capacitors also work. Avoid the 0805 size capacitors and C-packs. When placing AC coupling capacitors, symmetric placement is best. A capacitor value of 0.1 µF is best, and the value should match for the ±signal pair. The designer should place them along the TX pairs on the system board, which are usually routed on the top layer of the board.

The AC coupling capacitors have several placement options. Because the switch requires a bias voltage, the designer must place the capacitors on one side of the switch. If they are placed on both sides of the switch, a biasing voltage should be provided. Figure 4 shows a few placement options. The coupling capacitors are placed between the switch and endpoint. In this situation, the switch is biased by the system/host controller.

HD3SS3212 HD3SS3212I sch_ac_switch_ep_lase74.gifFigure 4. AC Coupling Capacitors between Switch TX and Endpoint TX

In Figure 5, the coupling capacitors are placed on the host transmit pair and endpoint transmit pair. In this situation, the switch on top is biased by the endpoint and the lower switch is biased by the host controller.

HD3SS3212 HD3SS3212I sch_ac_host_ep_lase74.gifFigure 5. AC Coupling Capacitors on Host TX and Endpoint TX

In the case where the common mode voltage in the system is higher than 2 V, the coupling capacitors are placed on both sides of the switch (shown in Figure 6). A biasing voltage of <2 V is required in this case.

HD3SS3212 HD3SS3212I sch_ac_both_lase74.gifFigure 6. AC Coupling Capacitors on Both Sides of Switch

The HD3SS3212 can be used with the USB Type C connector to support the connector’s flip ability. Figure 7 provides the generic location for the AC coupling capacitors for this application.

HD3SS3212 HD3SS3212I sch_ac_for_USB_C_lase74.gifFigure 7. AC Coupling Capacitors for USB Type C

11.2 Typical Applications

11.2.1 Down Facing Port for USB3.1 Type C

HD3SS3212 HD3SS3212I app_down_facing_LASE74.gifFigure 8. Down Facing Port for USB3.1 Type C Connector

11.2.1.1 Design Requirements

The HD3SS3212 can be designed into many different applications. All the applications have certain requirements for the system to work properly. The HD3SS3212 requires 3.3-V ±10% VCC rail. The OEn pin must be low for device to work otherwise it disables the outputs. This pin can be driven by a processor. The expectation is that one side of the device has AC coupling capacitors. Table 2 provides information on expected values to perform properly.

Table 2. Design Parameters

DESIGN PARAMETER VALUE
VCC 3.3 V
AXp/n, BXp/n, CXp/n CM input voltage 0 to 2 V
Control/OEn pin max voltage for low 0.8 V
Control/OEn pin min voltage for high 2.0 V
AC coupling capacitor 100 nF
RBIAS (Figure 8) when needed 1 kΩ

11.2.1.2 Detailed Design Procedure

The HD3SS3212 is a high-speed passive switch device that can behave as a mux or demux. Because this is a passive switch, signal integrity is important because the device provides no signal conditioning capability. The device can support 2 to 3 inches of board trace and a connector on either end.

To design in the HD3SS3212, the designer needs to understand the following.

  • Determine the loss profile between circuits that are to be muxed or demuxed.
  • Provide clean impedance and electrical length matched board traces.
  • Depending upon the application, determine the best place to put the 100-nF coupling capacitor.
  • Provide a control signal for the SEL and OEn pins.
  • The thermal pad must be connected to ground.
  • See the application schematics on recommended decouple capacitors from VCC pins to ground

11.2.1.3 Application Curves

HD3SS3212 HD3SS3212I app_eye_01_LASE74.gifFigure 9. 10 Gbps Source Eye Diagram
HD3SS3212 HD3SS3212I app_eye_02_LASE74.gifFigure 10. 10 Gbps Output Eye Diagram

11.2.2 Up Facing Port for USB3.1 Type C

HD3SS3212 HD3SS3212I app_up_facing_LASE74.gifFigure 11. Up Facing Port for USB3.1 USB Type-C Connector

11.2.3 PCIE/SATA/USB

HD3SS3212 HD3SS3212I app_PCIE_mthrbd_LASE74.gifFigure 12. PCIE Motherboard

11.2.4 PCIE/eSATA

HD3SS3212 HD3SS3212I app_PCIE_eSATA_LASE74.gifFigure 13. PCIE and eSATA Combo

11.2.5 USB/eSATA

HD3SS3212 HD3SS3212I app_eSATA_USB3_LASE74.gifFigure 14. eSATA and USB 3.0 Combo Connector

11.2.6 MIPI Camera Serial Interface

HD3SS3212 HD3SS3212I app_CSI_camera_LASE74.gifFigure 15. CSI Camera Array