ZHCSKV8A November 2020 – June 2022 DLP670S
PRODUCTION DATA
The device markings include both human-readable information and a 2-dimensional matrix code. The human-readable information is described in Figure 11-2. The 2-dimensional matrix code is an alpha-numeric character string that contains the DMD part number, Part 1 of Serial Number, and Part 2 of Serial Number. The first character of the DMD Serial Number (part 1) is the manufacturing year. The second character of the DMD Serial Number (part 1) is the manufacturing month.
Example: DLP670SFYR GHXXXXX LLLLLLM
Figure 11-2 DMD Marking Locations