ZHCSF60K June 2016 – July 2020 BQ77904 , BQ77905
PRODUCTION DATA
The BQ77904 supports 3-S and 4-S packs, while the BQ77905 supports 3-S, 4-S, and 5-S packs. To avoid accidentally detecting a UV fault on unused (shorted) cell inputs, the device must be configured for the specific cell count of the pack. This is set with the configuration pin, CCFG, which is mapped as in Table 8-5. The device periodically checks the CCFG status and takes tCCFG_DEG time to detect the pin status.
CCFG | CONFIGURATION | CONNECT TO |
---|---|---|
< VCCFGL for tCCFG_DEG | 3 cells | AVSS |
Within VCCFGM for tCCFG_DEG | 4 cells | AVDD |
> VCCFGH for tCCFG_DEG | 5 cells | Floating |
The CCFG pin should be tied to the recommended net from Table 8-5. The device compares the CCFG input voltage to the AVDD voltage and should never be set above the AVDD voltage. When the device configuration is for 5 S, leave the CCFG pin floating. The internal pin bias is approximately 30% of the AVDD voltage for the 5-S configuration. Note that the BQ77904 should not be configured in 5-S mode, as this results in a permanent UV fault.