SLUSG28 August 2025 BQ25176K
PRODUCTION DATA
请参考 PDF 数据表获取器件具体的封装图。
During normal operation, the OUT current should be regulated to the ISET programmed value. However, if a short circuit occurs on the ISET pin, the OUT current may rise to an unintended level. If the current at the OUT pin exceeds IOUT_OCP, the device turns off after a deglitch, tOUT_OCP_DGL. The safety timer resets the count, and the device remains latched off. An input supply or TS pin toggle is required to restart operation.
Figure 6-4 Overcurrent Protection