ZHCSH87B September 2017 – February 2020 TMP461-SP
PRODUCTION DATA.
The status register reports the state of the temperature ADC, the temperature limit comparators, and the connection to the remote sensor. Table 6 lists the status register bits. The status register is read-only and is read by accessing pointer address 02h.
STATUS REGISTER (Read = 02h, Write = N/A) | ||
---|---|---|
BIT NUMBER | BIT NAME | FUNCTION |
7 | BUSY | = 1 when the ADC is converting |
6 | LHIGH(1) | = 1 when the local high temperature limit is tripped |
5 | LLOW(1) | = 1 when the local low temperature limit is tripped |
4 | RHIGH(1) | = 1 when the remote high temperature limit is tripped |
3 | RLOW(1) | = 1 when the remote low temperature limit is tripped |
2 | OPEN(1) | = 1 when the remote sensor is an open circuit |
1 | RTHRM | = 1 when the remote THERM limit is tripped |
0 | LTHRM | = 1 when the local THERM limit is tripped |
The BUSY bit = 1 if the ADC is making a conversion. This bit is set to 0 if the ADC is not converting.
The LHIGH and LLOW bits indicate a local sensor overtemperature or undertemperature event, respectively. The RHIGH and RLOW bits indicate a remote sensor overtemperature or undertemperature event, respectively. The HIGH bit is set when the temperature exceeds the high limit in alert mode and therm mode and the low bit is set when the temperature goes below the low limit in alert mode. The OPEN bit indicates an open-circuit condition on the remote sensor. When pin 7 is configured as the ALERT output, the five flags are NORed together. If any of the five flags are high, the ALERT interrupt latch is set and the ALERT output goes low. Reading the status register clears the five flags, provided that the condition that caused the setting of the flags is not present anymore (that is, the value of the corresponding result register is within the limits, or the remote sensor is connected properly and functional). The ALERT interrupt latch (and the ALERT pin correspondingly) is not reset by reading the status register. The reset is done by the master reading the temperature sensor device address to service the interrupt, and only if the flags are reset and the condition that caused them to be set is no longer present.
The RTHRM and LTHRM flags are set when the corresponding temperature exceeds the programmed THERM limit. These flags are reset automatically when the temperature returns to within the limits. The THERM output goes low in the case of overtemperature on either the local or remote channel, and goes high as soon as the measurements are within the limits again. The THERM hysteresis register (21h) allows hysteresis to be added so that the flag resets and the output goes high when the temperature returns to or goes below the limit value minus the hysteresis value.
When pin 7 is configured as THERM2, only the high limits matter. The LHIGH and RHIGH flags are set if the respective temperatures exceed the limit values, and the pin goes low to indicate the event. The LLOW and RLOW flags have no effect on THERM2 and the output behaves the same way when configured as THERM.