ZHCS834G June 2011 – March 2020 TPS7A63-Q1 , TPS7A6401-Q1
PRODUCTION DATA.
When using the TPS7A6333-Q1, TPS7A6350-Q1, TI recommends adding a 10-µF to 22-µF capacitor to the input to keep the input voltage stable. TI also recommends adding a 1-µF to 10-µF low ESR ceramic capacitor to get a stable output.
The reset delay time is set by an external capacitor (CDLY) to ground, capacitor value typical from 100 pF to
100 nF. Equation 1 provides the method for the calculation.
Connecting an external resistor to ground at the ROSC pin can set the duration of the watchdog window. Equation 4 provides the method for the calculation. Usually a 10-kΩ to 200-kΩ resistor can be used to set the time.