SNVSA75D November 2015 – May 2017
PRODUCTION DATA.
The LP8862-Q1 device is designed to operate from an automotive battery. The device must be protected from reversal voltage and voltage dump over 50 V. The resistance of the input supply rail must be low enough so that the input current transient does not cause too-high drop at the LP8862-Q1 VIN pin. If the input supply is connected by using long wires additional bulk capacitance may be required in addition to the ceramic bypass capacitors in the VIN line.