SLAA380B December 2007 – September 2018 MSP430F2616 , MSP430F2617 , MSP430F2618 , MSP430F2619
Both MSP430F16x and MSP430F261x have 256 bytes of information flash memory located in the memory range of 0x1000 to 0x10FF. While the total memory size is the same, the memory is organized differently. The MSP430F16x device information memory consists of two flash segments (INFOA and INFOB) that are 128 bytes each, and the MSP430F261x has four segments (INFOA, INFOB, INFOC, and INFOD) that are 64 bytes each.
Applications storing data in the information memory need to consider the different segment sizes. Each information flash memory segment must be erased individually, resulting in four write accesses on an MSP430F261x instead of two on the MSP430F16x. Also, note that the MSP430F261x INFOA segment is protected by a lock feature and requires special treatment to be erased or written to. However, in general it is not recommended to erase INFOA or store any user data in it. INFOA comes with factory-provided device-specific calibration data, such as calibration to generate specific frequencies using the DCO. The majority of applications can benefit from those constants.
See the MSP430x2xx Family User’s Guide for more details on the organization of the 2xx information flash memory, the INFOA lock feature, and the factory-provided calibration constants. [2]