ZHCSDZ1D July 2015 – January 2022 TUSB4020BI
PRODUCTION DATA
PIN | TYPE(1) | DESCRIPTION | ||||||||
---|---|---|---|---|---|---|---|---|---|---|
NAME | NO. | |||||||||
CLOCK AND RESET SIGNALS | ||||||||||
GRSTz | 11 | I PU |
Global power reset. This reset brings all of the TUSB4020BI internal registers to their default states. When GRSTz is asserted, the device is completely nonfunctional. | |||||||
XI | 38 | I | Crystal input. This terminal is the crystal input for the internal oscillator. The input may alternately be driven by the output of an external oscillator. | |||||||
XO | 39 | O | Crystal output. This terminal is the crystal output for the internal oscillator. If XI is driven by an external oscillator this pin may be left unconnected. | |||||||
USB UPSTREAM SIGNALS | ||||||||||
USB_DP_UP | 26 | I/O | USB high-speed differential transceiver (positive) | |||||||
USB_DM_UP | 27 | I/O | USB high-speed differential transceiver (negative) | |||||||
USB_R1 | 24 | I | Precision resistor reference. A 9.53-kΩ ±1% resistor should be connected between USB_R1 and GND. | |||||||
USB_VBUS | 9 | I | USB upstream port power monitor.
The VBUS detection requires a voltage divider. The
signal USB_VBUS must be connected to VBUS through
a 90.9-kΩ ±1% resistor, and to ground through a
10-kΩ ±1% resistor from the signal to ground. |
|||||||
USB DOWNSTREAM SIGNALS | ||||||||||
USB_DP_DN1 | 41 | I/O | USB high-speed differential transceiver (positive) downstream port 1. | |||||||
USB_DM_DN1 | 42 | I/O | USB high-speed differential transceiver (negative) downstream port 1. | |||||||
PWRCTL1/BATEN1 | 4 | I/O PD |
USB port 1 power-on control for downstream power or battery charging enable. The terminal is used for control of the downstream power switch for Port 1. | |||||||
In addition, the value of the terminal is sampled at the deassertion of reset to determine the value of the battery charging support for Port 1 as indicated in the Battery Charging Support register. | ||||||||||
0 = Battery
charging not supported 1 = Battery charging supported |
||||||||||
OVERCUR1z | 5 | I PU |
USB DS port 1 overcurrent detection input. This terminal is used to connect the over current output of the downstream port power switch for port 1. | |||||||
0 = An
overcurrent event has occurred 1 = An overcurrent event has not occurred |
||||||||||
If power management is enabled, the external circuitry needed should be determined by the power switch. In ganged mode, either OVERCUR1z or OVERCUR2z can be used. In ganged mode, the overcurrent will be reported as a hub event instead of a port event. | ||||||||||
USB_DP_DN2 | 14 | I/O | USB high-speed differential transceiver (positive) downstream port 2. | |||||||
USB_DM_DN2 | 15 | I/O | USB high-speed differential transceiver (negative) downstream port 2. | |||||||
PWRCTL2/BATEN2 | 6 | I/O PD |
Power-on control /battery charging enable for downstream port 2. This terminal is used for control of the downstream power switch for port 2. | |||||||
The value of the terminal is sampled at the deassertion of reset to determine the value of the battery charging support for port 2 as indicated in the Battery Charging Support register. | ||||||||||
0 = Battery charging
not supported 1 = Battery charging supported |
||||||||||
OVERCUR2z | 8 | I PU |
Overcurrent detection for downstream port 2. This terminal is used to connect the over current output of the downstream port power switch for port 2. | |||||||
0 = An
overcurrent event has occurred 1 = An overcurrent event has not occurred |
||||||||||
If power management is enabled, the external circuitry needed should be determined by the power switch. In ganged mode either OVERCUR1z or OVERCUR2z can be used. In ganged mode the overcurrent will be reported as a hub event instead of a port event. | ||||||||||
I2C/SMBUS SIGNALS | ||||||||||
SCL/SMBCLK | 2 | I/O PD |
I2C clock/SMBus clock. Function of terminal depends on the setting of the SMBUSz input. | |||||||
When SMBUSz = 1, this terminal acts as the serial clock interface for an I2C EEPROM. | ||||||||||
When SMBUSz = 0, this terminal acts as the serial clock interface for an SMBus host. | ||||||||||
This pin must be pulled up to use the OTP ROM. | ||||||||||
Can be left unconnected if external interface not implemented. | ||||||||||
SDA/SMBDAT | 3 | I/O PD |
I2C data/SMBus data. Function of terminal depends on the setting of the SMBUSz input. | |||||||
When SMBUSz = 1, this terminal acts as the serial data interface for an I2C EEPROM. | ||||||||||
When SMBUSz = 0, this terminal acts as the serial data interface for an SMBus host. | ||||||||||
This pin must be pulled up to use the OTP ROM. | ||||||||||
Can be left unconnected if external interface not implemented. | ||||||||||
TEST AND MISCELLANEOUS SIGNALS | ||||||||||
SMBUSz | 22 | I PU |
SMBUS mode. | |||||||
The value of the terminal is sampled at the deassertion of reset to enable I2C or SMBus mode. | ||||||||||
0 = SMBus mode
selected 1 = I2C mode selected |
||||||||||
After reset, this signal is driven low by the TUSB4020BI. Due to this behavior, it is recommended to not tie directly to supply but instead pull-up or pull-down using external resistor. | ||||||||||
PWRCTL_POL | 21 | I/O PD |
Power control polarity. | |||||||
The value of the terminal is sampled at the deassertion of reset to set the polarity of PWRCTL[2:1]. | ||||||||||
0 = PWRCTL polarity is
active high. 1 = PWRCTL polarity is active low. |
||||||||||
After reset, this signal is driven low by the TUSB4020BI. Due to this behavior, it is recommended to not tie directly to supply but instead pull-up or pull-down using external resistor. | ||||||||||
GANGED/SMBA2/ HS_UP |
35 | I PU |
Ganged operation enable/SMBus address bit 2/ high-speed status for upstream port | |||||||
The value of the terminal is sampled at the deassertion of reset to set the power switch and over current detection mode as follows: | ||||||||||
0 = Individual power
control supported when power switching is
enabled. 1 = Power control gangs supported when power switching is enabled. |
||||||||||
When SMBus mode is enabled using SMBUSz, this terminal sets the value of the SMBus slave address bit 2. SMBus slave address bit 3 is always 1 for the TUSB4020BI. | ||||||||||
After reset, this signal indicates the high-speed USB connection status of the upstream port. A value of 1 indicates the upstream port is connected to a high-speed USB capable port. | ||||||||||
Note: Individual power control must be enabled for battery charging applications. | ||||||||||
FULLPWRMGMTz/ SMBA1 |
36 | I, PU | Full power management enable/ SMBus Address bit 1. | |||||||
The value of the terminal is sampled at the deassertion of reset to set the power switch control follows: | ||||||||||
0 = Power switching
supported 1 = Power switching not supported |
||||||||||
Full power management is the ability to control power to the downstream ports of the TUSB4020BI using PWRCTL[2:1]/BATEN[2:1]. | ||||||||||
When SMBus mode is enabled using SMBUSz, this terminal sets the value of the SMBus slave address bit 1. SMBus slave address bit 3 is always 1 for the TUSB4020BI. | ||||||||||
Can be left unconnected if full power management and SMBus are not implemented. | ||||||||||
After reset, this signal is driven low by the TUSB4020BI. Due to this behavior, it is recommended to not tie directly to supply but instead pull-up or pull-down using external resistor. | ||||||||||
Note: Power switching must be supported for battery charging applications. | ||||||||||
RSVD | 16, 17, 19, 20, 28, 29, 31, 32, 43, 44, 46, 47 | I/O | Reserved. These pins are for internal use only and should be left unconnected on PCB. | |||||||
TEST | 10 | I PD |
TEST mode enable. When this terminal is asserted high at reset enables test mode. This terminal is reserved for factory use. It is recommended to pull-down this terminal to ground. | |||||||
POWER AND GROUND SIGNALS | ||||||||||
VDD | 1, 12, 18, 30, 34, 45 | PWR | 1.1-V power rail | |||||||
VDD33 | 7, 13, 23, 25, 33, 37, 40, 48 | PWR | 3.3-V power rail | |||||||
GND | PAD | — | Ground |