ZHCSI98E November 2010 – March 2020 TPS7A6201-Q1
PRODUCTION DATA.
请参考 PDF 数据表获取器件具体的封装图。
For the LDO power supply, especially these high voltage and large current ones, layout is an important step. If layout is not carefully designed, the regulator could not deliver enough output current because of the thermal limitation. To improve the thermal performance of the device, and maximize the current output at high ambient temperature, TI recommends spreading the thermal pad as large as possible and place enough thermal vias on the thermal pad. Figure 25 provides an example layout.