ZHCSB48B May 2013 – January 2019 TPS55330
PRODUCTION DATA.
The TPS55330 has internal slope compensation to prevent subharmonic oscillations. The sensed current slope of boost converter can be expressed as Equation 4:
The slope compensation dv/dt can be calculated using Equation 5.
In a converter with current mode control, in addition to the output voltage feedback loop, the inner current loop including the inductor current sampling effect as well as the slope compensation on the small signal response should be taken into account, which can be modeled as seen in Equation 6:
where
NOTE
If Sn << Se, the converter operates in voltage mode control rather than current mode control, and Equation 6 is no longer valid.