ZHCSCE7I March 2014 – July 2019 TPS23861
PRODUCTION DATA.
Command = 0Ah with 1 Data Byte, Read Only
Command = 0Bh with 1 Data Byte, Clear on Read
BITS | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 |
---|---|---|---|---|---|---|---|---|
BIT NAME | TSD | - | VDUV | VPUV | - | - | - | - |
POR VALUE | 0 | 0 | 1 | 1 | 0 | 0 | 0 | 0 |
Active high, each bit corresponds to a particular event that occurred.
A read at each location (0Ah or 0Bh) returns the same register data with the exception that the Clear-on-Read command clears all bits of the register.
If this register is causing the INT pin to be activated, this Clear-on-Read releases the INT pin.
Any active bit has an impact on Interrupt Register as indicated in the Interrupt Register description.
Bit Descriptions
TSD: Indicates that a thermal shutdown occurred. When there is thermal shutdown, all ports are powered off and are put in Off Mode. The TPS23861 internal circuitry continues to operate however, including the A/D converters. Note that at as soon as the internal temperature has decreased below the low threshold, the ports can be powered on regardless of the status of the TSD bit.
1 = Thermal shutdown occurred.
0 = No thermal shutdown occurred.
VDUV: Indicates that a VDD UVLO occurred. VDUV is set following a power-on reset or if the voltage at the VDD pin falls below VUVDD_F
1 = VDD UVLO occurred.
0 = No VDD UVLO occurred.
VPUV: Indicates that a VPWR UVLO occurred. VPUV is set following a power-on reset or if the voltage at the VPWR pin falls below VPUV_F.
1 = VPWR undervoltage occurred.
0 = No VPWR undervoltage occurred.
NOTE
If the RESET input is pulled low during normal operation, VPUV is set if VPWR is below its UVLO threshold. There is no impact on VDUV since VDD is maintained.
When VPWR drops below VPUV_F but not as low as VUVLOPW_F all ports are powered off as if a push-button off was executed. (Same as writing 1 to POFFn in Power Enable Register.) When VPWR undervoltage (below VUVLOPW_F) occurs, all ports are powered off, and there is a power-on reset.