ZHCSCG1C April 2014 – July 2015 TMP007
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TMP007 is a complete IR thermopile sensor system on a chip that includes the sensing element, signal conditioner, ADC, and math engine to calculate object and die temperatures. The TMP007 is ideal for applications where the object cannot be placed in thermal contact with a conventional temperature sensor. Common reasons for noncontact temperature sensing are:
For this application, the system must operate over the environment described in Table 10.
DESIGN PARAMETER | EXAMPLE VALUE | COMMENT |
---|---|---|
N | 32 | Number of devices in calibration set |
Minimum TDIE | 0°C | Minimum expected die temperature |
Maximum TDIE | 60°C | Maximum expected die temperature |
Minimum TOBJ | 0°C | Minimum expected objected temperature |
Maximum TOBJ | 60°C | Maximum expected object temperature |
ε | 0.95 | Object emissivity |
Field of view | 110° | Field of view subtended by object |
Conversion rate | 1 sample/second |
Select a set of values for TDIE and TOBJ to generate the calibration set. At a minimum, include the four extreme points of the temperature ranges desired. In practice, it is best to include a number of intermediate points as well. This example uses the values shown in Table 11, with an X marking the values chosen for measurement.
TOBJ | TDIE | |||
---|---|---|---|---|
0°C | 20°C | 40°C | 60°C | |
0°C | X | X | X | X |
20°C | X | X | X | X |
40°C | X | X | X | X |
60°C | X | X | X | X |
Before attempting to calibrate the system, it is necessary to establish the stability of the system. Noise is a measure of precision, which is the random deviation from the mean of the distribution. For a Gaussian (or normal) distribution, the precision is typically characterized by the standard deviation (sensor noise), σ.
To begin calibration, select an object temperature (TOBJ) and a value for the die temperature (TDIE). With these system temperatures stable, take a statistically significant number of samples of VSensor (results shown in register 00h).
in this example, 64 samples were taken. Do not use the object temperature readings given in register 03h; these values are invalid before calibration.
To compensate for first order drift in system temperatures, it is often useful to normalize the data set. For this purpose, for each temperature set, the sensor voltage data (given in register 00h) is normalized by first finding the best fit line of the form shown in Equation 11:
The normalized data for each data set is then calculated as shown in Equation 12:
The normalized data, VSensor_norm, is centered on zero mean, and is first-order corrected for long-term drift. The standard deviation for each data set is then calculated to estimate the sensor noise, σ. Verify that the data are limited by white noise and no other effects. For a sensor-noise-limited data set, vSENSOR σ is typically < 1 μV, and preferably < 0.5 μV after first-order correction for drift, as described previously. If this condition is not satisfied, then the calibration accuracy is limited by external system factors (for example, convection or conduction). Repeat this process for each combination of TOBJ and TDIE for which the calibration is to be performed. The normalized data are used only for evaluating the suitability of the data set for calibration, and not for the actual calibration itself.
For calibration, the mean value, <VSENSOR>, is calculated for each combination of TOBJ and TDIE, as shown in Table 12. Using the mean value minimizes error introduced by random noise. Based on the means, a set of coefficients is generated based on a user-selected optimization criteria for Equation 7. Common criteria are minimizing the maximum error, minimizing the average error, and so on. For a detailed discussion of optimization methods, see SBOU142 — TMP007 Calibration Guide.
TOBJ | TDIE | |||
---|---|---|---|---|
0°C | 20°C | 40°C | 60°C | |
0°C | <VSENSOR> | <VSENSOR> | <VSENSOR> | <VSENSOR> |
20°C | <VSENSOR> | <VSENSOR> | <VSENSOR> | <VSENSOR> |
40°C | <VSENSOR> | <VSENSOR> | <VSENSOR> | <VSENSOR> |
60°C | <VSENSOR> | <VSENSOR> | <VSENSOR> | <VSENSOR> |
The next step is to use the generated coefficients to verify the calibration, and determine the accuracy of the system. For common calibration (C) , the same coefficients are used for all devices; in unit calibration (U) the coefficients are calculated for each device. Common calibration includes device-to-device variation, and thus is less accurate, but much easier to implement. Unit calibration is more accurate, and eliminates device variation, but requires more effort to implement. The choice depends on the application requirements for accuracy versus implementation effort.
Mean calibration error at each point is defined as shown in Equation 13:
where
The mean error graph (see Figure 54) provides an efficient method of understanding how the systematic errors vary across the temperature ranges of interest. This graph also provides a means of weighing the benefits and efforts of common versus unit calibration for a particular application.
Note that calibration does not affect the temporal random noise observed, as shown in Figure 55. The standard deviation of the temperature error is independent of the calibration if the random error is dominated by the sensor noise and not external system factors, such as convection and conduction. For common calibration, the total standard deviation increases because of the effects of device-to-device variation. This standard deviation is calculated in the usual way, by substituting TOBJ_PREDICT for the mean in the standard deviation formula.
The accuracy is then defined as the mean calibration error plus the random errors from all sources. For this example application, use the criteria shown in Equation 14:
The resulting accuracy over TOBJ and TDIE is shown in Figure 10 and Figure 11 for the unit- and common-calibration approaches, respectively. Clearly, the unit calibration results in higher accuracy, though common calibration is applicable for many application requirements.
For this application, the system must operate over the environment described in Table 13.
DESIGN PARAMETER | EXAMPLE VALUE | COMMENT |
---|---|---|
N | 16 | Number of devices in calibration set |
Minimum TDIE | 25°C | Minimum expected die temperature |
Maximum TDIE | 30°C | Maximum expected die temperature |
Minimum TOBJ | 33°C | Minimum expected objected temperature |
Maximum TOBJ | 41°C | Maximum expected object temperature |
ε | 0.95 | Object emissivity |
Field of view | 110° | Field of view subtended by object |
Conversion rate | 1 sample/second |
Select a set of values for TDIE and TOBJ to generate the calibration set. At a minimum, include the four extreme points of the temperature ranges desired. In practice, it is best to include a number of intermediate points as well. This example uses the values shown in Table 14, with an X marking the values chosen for measurement. In this application, the calibration set is weighted more densely around the region of interest.
Before attempting to calibrate the system, it is necessary to establish the stability of the system. Noise is a measure of precision, which is the random deviation from the mean of the distribution. For a Gaussian (or normal) distribution, the precision is typically characterized by the standard deviation (sensor noise), σ.
To begin calibration, select an object temperature (TOBJ) and a value for the die temperature (TDIE). With these system temperatures stable, take a statistically significant number of samples of VSensor (results shown in register 00h).
in this example, 64 samples were taken. Do not use the object temperature readings given in register 03h; these values are invalid before calibration.
To compensate for first order drift in system temperatures, it is often useful to normalize the data set. For this purpose, for each temperature set, the sensor voltage data (given in register 00h) is normalized by first finding the best fit line of the form shown in Equation 15:
The normalized data for each data set is then calculated as shown in Equation 16:
The normalized data, VSensor_norm, is centered on zero mean, and is first-order corrected for long-term drift. The standard deviation for each data set is then calculated to estimate the sensor noise, σ. Verify that the data are limited by white noise and no other effects. For a sensor-noise-limited data set, vSENSOR σ is typically < 1 μV, and preferably < 0.5 μV after first-order correction for drift, as described previously. If this condition is not satisfied, then the calibration accuracy is limited by external system factors (for example, convection or conduction). Repeat this process for each combination of TOBJ and TDIE for which the calibration is to be performed. The normalized data are used only for evaluating the suitability of the data set for calibration, and not for the actual calibration itself.
For calibration, the mean value, <VSENSOR>, is calculated for each combination of TOBJ and TDIE, as shown in Table 15. Using the mean value minimizes error introduced by random noise. Based on the means, a set of coefficients is generated based on a user-selected optimization criteria for Equation 7. Common criteria are minimizing the maximum error, minimizing the average error, and so on. For a detailed discussion of optimization methods, see SBOU142 — TMP007 Calibration Guide.
The next step is to use the generated coefficients to verify the calibration, and determine the accuracy of the system. For common calibration (C) , the same coefficients are used for all devices; in unit calibration (U) the coefficients are calculated for each device. Common calibration includes device-to-device variation, and thus is less accurate, but much easier to implement. Unit calibration is more accurate, and eliminates device variation, but requires more effort to implement. The choice depends on the application requirements for accuracy versus implementation effort.
Mean calibration error at each point is defined as shown in Equation 17:
where
The mean error graph (see Figure 54) provides an efficient method of understanding how the systematic errors vary across the temperature ranges of interest. This graph also provides a means of weighing the benefits and efforts of common versus unit calibration for a particular application.
Note that calibration does not affect the temporal random noise observed, as shown in Figure 55. The standard deviation of the temperature error is independent of the calibration if the random error is dominated by the sensor noise and not external system factors, such as convection and conduction. For common calibration, the total standard deviation increases because of the effects of device-to-device variation. This standard deviation is calculated in the usual way, by substituting TOBJ_PREDICT for the mean in the standard deviation formula.
The accuracy is then defined as the mean calibration error plus the random errors from all sources. For this example application, use the criteria shown in Equation 14:
The resulting accuracy over TOBJ and TDIE is shown in Figure 57 for the unit- and common-calibration approaches. Clearly, the unit calibration results in higher accuracy, though common calibration is applicable for many application requirements.
Reduce the random temporal error by increasing the sample time. Figure 58 shows the effects of increasing the sample time on the standard deviation. As a result of device-to-device variation, the effects of increased sample time on the common-calibration scheme is negligible; however, an improvement is seen for the unit calibration scheme.
Finally, the resulting accuracy is shown for the different sample times as a function of TDIE in Figure 59. Improve the accuracy by generating separate coefficient sets for TDIE = 25°C and TDIE = 30°C.
It is often necessary to estimate system performance as part of the design process. A key system parameter is temperature accuracy for a given set of parameters. Table 16 lists example parameters for estimating system performance.
DESIGN PARAMETER | EXAMPLE VALUE | COMMENT |
---|---|---|
Object distance | 10 mm | Distance to object |
Object diameter | 15 mm | Object size and geometry |
ε | 0.95 | Object emissivity |
TDIE | 23°C | Die temperature |
TOBJ | 30°C | Maximum expected object temperature |
FOV | 110° | Field of view subtended by object |
Responsivity (R0) | 10.8 V/W | Responsivity for TDIE = 25°C, θ = 0° |
Responsivity (R) | 9 V/W | Responsivity for 110° FOV |
Sensor rms noise | 0.20 µV | RMS sensor noise at TDIE = 25°C |
NEP | 30 nW | Thermal power equivalent to rms sensor noise |
Conversion rate | 1 SPS | SPS = samples per second |
The system accuracy is a function of TOBJ, TDIE, ε, and radiation transfer.
The radiation transfer factor is system dependent, and is affected by the object distance and geometry (for example, planar versus curved surfaces, or presence of lenses). For an planar object perpendicular to the detector axis (see Figure 19), the radiation transfer follows the well-known sin2(θ) result. This expression can be used with a radiation transfer function responsivity value of 9 V/W to estimate system performance.
Because of the angular dependence of the TMP007 detector response, a more accurate representation for the same radiative transfer function geometry is shown in Equation 19:
where
The responsivity value of 9 V/W is based on a system with a 110° FOV.
Using the device-specific radiation transfer expression and R0, the detector response is shown in Equation 20:
where
The value of cos θ is shown in Equation 21:
where
Differentiating with respect to object temperature, a small change in temperature creates a small change in the measured voltage given by Equation 22:
Substituting values for the parameters yields Equation 23:
Based on Figure 4, the sensor rms noise at TDIE = 25°C is ~0.25 µV; thus, the rms variation in temperature measurement is as shown in Equation 24:
The peak-to-peak noise is approximately six times the rms noise; therefore, estimate an accuracy of approximately ±0.33°C.
This estimate can also be made using the noise-equivalent power (NEP), noting that NEP is the ratio of noise to responsivity, as shown in Equation 25:
Assuming the system is sensor-noise limited, then from Figure 5, the NEP is ~30 nW at 25°C, as shown in Equation 26:
Again, the peak-to-peak noise is approximately 6X the rms noise; therefore estimate an accuracy of approximately ±0.42°C.
The different results from these two techniques is because of estimated values used for some parameters. The purpose of these techniques is not to obtain exact answers, but rather to quickly estimate the feasibility of a system implementation based on basic system parameters. These examples are intended only as guidelines; the specific values for the parameters depend on the specific system details.