ZHCSJU8G February 2011 – March 2022 LM21215
PRODUCTION DATA
The PGOOD pin provides the user with a way to monitor the status of the LM21215. In order to use the PGOOD pin, the application must provide a pullup resistor to a desired DC voltage (in other words, VIN). PGOOD will respond to a fault condition by pulling the PGOOD pin low with the open-drain output. PGOOD pulls low on the following conditions:
Figure 7-2 shows the conditions that will cause PGOOD to fall.