ZHCSJU8G February 2011 – March 2022 LM21215
PRODUCTION DATA
The LM21215 offers increased efficiency when operating at light loads. Whenever the load current is reduced to a point where the peak to peak inductor ripple current is greater than two times the load current, the device will enter the diode emulation mode, preventing significant negative inductor current. The point at which this occurs is the critical conduction boundary and can be calculated with Equation 1:
It can be seen that in diode emulation mode, whenever the inductor current reaches zero, the SW node becomes high impedance. Ringing will occur on this pin as a result of the LC tank circuit formed by the inductor and the parasitic capacitance at the node. If this ringing is of concern, an additional RC snubber circuit can be added from the switch node to ground.
At very light loads, usually below 100 mA, several pulses can be skipped in between switching cycles, effectively reducing the switching frequency and further improving light-load efficiency.