ZHCSK67B June 2017 – August 2019 ADS1287
PRODUCTION DATA.
The WAKEUP command is used to exit standby mode and to resume normal operation. The STANDBY, WAKEUP sequence is illustrated in Figure 65. Figure 6 illustrates the time for new conversion data. After writing the ADC registers, the ADC restarts the filter cycle and, as a consequence, results in loss of the previous synchronization. In continuous synchronization mode, use the STANDBY, WAKEUP command sequence to restore the previous synchronization; see the Continuous-Sync Mode section for details.