• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Powering DRA821 with TPS6594-Q1 and LP8764-Q1

    • SLVUBY7A October   2020  – October 2022 DRA821U , DRA821U-Q1 , LP8764-Q1 , TPS6594-Q1

       

  • CONTENTS
  • SEARCH
  • Powering DRA821 with TPS6594-Q1 and LP8764-Q1
  1.   User's Guide for Powering DRA821 with TPS6594-Q1 and LP8764-Q1
  2.   Trademarks
  3. 1Introduction
  4. 2Device Versions
  5. 3Processor Connections
  6. 4Supporting Functional Safety Systems
    1. 4.1 Achieving ASIL-B System Requirements
    2. 4.2 Achieving up to ASIL-D System Requirements
  7. 5Static NVM Settings
    1. 5.1  Application-Based Configuration Settings
    2. 5.2  Device Identification Settings
    3. 5.3  BUCK Settings
    4. 5.4  LDO Settings
    5. 5.5  VCCA Settings
    6. 5.6  GPIO Settings
    7. 5.7  Finite State Machine (FSM) Settings
    8. 5.8  Interrupt Settings
    9. 5.9  POWERGOOD Settings
    10. 5.10 Miscellaneous Settings
    11. 5.11 Interface Settings
    12. 5.12 Multi-Device Settings
    13. 5.13 Watchdog Settings
  8. 6Pre-Configurable Finite State Machine (PFSM) Settings
    1. 6.1 Configured States
    2. 6.2 PFSM Triggers
    3. 6.3 Power Sequences
      1. 6.3.1 TO_SAFE_SEVERE
      2. 6.3.2 TO_SAFE_ORDERLY and TO_STANDBY
      3. 6.3.3 ACTIVE_TO_WARM
      4. 6.3.4 ESM_SOC_ERROR
      5. 6.3.5 PWR_SOC_ERROR
      6. 6.3.6 MCU_TO_WARM
      7. 6.3.7 TO_MCU
      8. 6.3.8 TO_ACTIVE
      9. 6.3.9 TO_RETENTION
  9. 7Application Examples
    1. 7.1 Moving Between States: ACTIVE, MCU, and RETENTION
      1. 7.1.1 ACTIVE
      2. 7.1.2 MCU ONLY
      3. 7.1.3 RETENTION
    2. 7.2 Entering and Exiting Standby
    3. 7.3 Entering and Existing LP_STANDBY
    4. 7.4 GPIO8 and Watchdog
  10. 8Additional Resources
  11. 9Revision History
  12. IMPORTANT NOTICE
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
USER'S GUIDE

Powering DRA821 with TPS6594-Q1 and LP8764-Q1

1 User's Guide for Powering DRA821 with TPS6594-Q1 and LP8764-Q1

This user’s guide can be used as a guide for integrating the TPS6594-Q1 and LP8764-Q1 power management integrated circuits (PMICs) into a system powering the DRA821 processor.

Trademarks

Jacinto™ is a trademark of Texas Instruments.

All trademarks are the property of their respective owners.

1 Introduction

This user’s guide defines the power distribution network (PDN) between the TPS6594-Q1 and LP8764-Q1 devices and the DRA821 processor. This document describes the platform power resource connections, digital control connections, and PMIC sequencing settings to support the different processor state transitions. The PMIC default non-volatile memory (NVM) settings, internal state transitions, and power sequences are also defined in this document. This user's guide does not provide information about the electrical characteristics, external components, package, or the functionality of the PMICs or processor. For such information and the full register maps, refer to the data sheet for each device. In the event of any inconsistency between the official specification and any user's guide, application report, or other referenced material, the data sheet specification is the definitive source.

2 Device Versions

There are different versions of the TPS6594-Q1 and LP8764-Q1 devices available with unique NVM settings to support different processor solutions. The unique NVM settings for each PMIC device are optimized per PDN design to support different processors, processing loads, SDRAM types, system functional safety levels, and end product features - such as low power modes, processor interface levels, SD Card, and so forth. The NVM settings can be distinguished using the TI_NVM_ID register. In this user guide, each PMIC device is distinguished by the TI orderable part number, TI_NVM_ID, and TI_NVM_REV values listed in Table 2-1.

Table 2-1 TPS6594-Q1 and LP8764-Q1 NVM Settings and Orderable Part Numbers
PDN USE CASE Orderable Part Number Device Mode TI_NVM_ID TI_NVM_REV
  • Up to 4.25 A(1) on the CORE rail
  • Up to 4.25 A(1) on the CPU rails
  • Up to 3.4 A(1) on the SDRAM, with support for LPDDR4
  • Supports Functional Safety up to ASIL-D level
  • Supports low power modes, including MCU-only, GPIO Retention, and DDR Retention states
  • Supports I/O level of 3.3 V or 1.8 V
  • Supports use of SD card
TPS6594141B

Primary

0x1B 0x01
LP876441B1 Secondary 0xB1 0x01
(1) TI recommends having 15% margin between the maximum expected load current and the maximum current allowed per each PMIC output rail.

3 Processor Connections

This section details how the TPS6594-Q1 and LP8764-Q1 power resources and GPIO signals are connected to the processor and other peripheral components to support the PDN use case.

Figure 3-1 shows the detailed power mapping between the processor and the TPS6594-Q1 and LP8764-Q1 PMICs. In this configuration, both PMICs use a 3.3 V input voltage. For Functional Safety applications, there is a protection FET before VCCA that connects to the OVPGDRV pin of the primary PMIC, allowing voltage monitoring of the input supply to the PMICs.

The VCCA voltage must be the first voltage applied to the PMIC devices. VIO_IN of the PMICs must be supplied after VCCA. In this configuration, VIO_IN is supplied by the load switch that also supplies the VDDSHVx_MCU voltage domain of the processor to allow the digital components of the PMIC devices (such as GPIOs) to remain supplied in MCU-only mode. Additionally, by controlling VIO_IN of both PMICs through this load switch, the system can also reduce power consumption in GPIO Retention or DDR Retention modes, since the load switch is disabled.

This PDN supports the use of either a single dual load switch (TPS22966-Q1) with an AEC-100 Grade 2 (-40 to +105°C) temperature rating or two single load switches (TPS22965-Q1) with an AEC-100 Grade 1 (-40 to +125°C) rating if a higher ambient temperature range is desired. The PDN diagrams of this section also include a few optional discrete power components to support additional system functions that may be needed. The TLV70033-Q1 LDO is used to support compliant USB data eye performance by supplying a low noise 3.3 V for USB 2.0 interface integration. The TLV70018-Q1 LDO is available to support on-board EFUSE programming on high security SoC PNs. Alternative LDOs can be chosen for SD card dual-voltage I/O support (3.3 V and 1.8 V), TLV7103318-Q1 dual-voltage LDO can be used to enable compliant, dual voltage, high-speed SD card operations.

Figure 3-1 TPS6594-Q1 and LP8764-Q1 Power Connections

The power resource assignments shown in Figure 3-1 enable the support for different processor low-power modes, including MCU-only mode, GPIO Retention, and DDR Retention. Please use Table 3-1 as a guide to understand which power resources are required to support different system features. If the system feature listed is not required, the power resource connection can be removed.

Table 3-1 Power Resources by System Power States
DevicePMIC ResourceProcessor DomainsPower States
Active SoCMCU - onlyGPIO RetentionDDR Retention
TPS6594-Q1BUCK1VDDA_xRequiredRequired
BUCK2VDDSHVx_MCU (1.8V)RequiredRequired
BUCK3VDD_MCU, VDDAR_MCURequiredRequired
BUCK4VDDS_DDR_BIAS, VDDS_DDR_IORequiredRequired
BUCK5VDDA_1P8_PHYsRequired
LDO1N/ARequiredRequired
LDO2VDDA_0P8_PLLs/DLLsRequired
LDO3VDD_WAKE0RequiredRequired
LDO4VDDA_1P8_PLLsRequired
LP8764-Q1BUCK1VDD_CPURequired
BUCK2VDDAR_CPU/CORERequired
BUCK3VDD_CORE, VDDA_0P8_PHYsRequired
BUCK4VDDS_MMC0Required
TPS22965-Q1Load SwitchVDDSHVx_MCU (3.3 V)RequiredRequired
TPS22966-Q1Load Switch 1VDDSHV0(1)Required
Load Switch 2VDDSHV2Required
(1) VDDSHV5 can also be powered by this rail if an SD card is not required in the system.

Figure 3-2 shows the digital control signal mapping between the processor and the PMIC devices. For the two PMIC devices to work together, the primary PMIC and secondary PMIC must establish an SPMI communication channel. The SPMI bus allows the TPS6594-Q1 and LP8764-Q1 to synchronize their internal Pre-Configurable State Machines (PFSM) so that they operate as one PFSM across all power and digital resources. The GPIO_5 and GPIO_6 pins on the TPS6594-Q1 and GPIO_8 and GPIO_9 pins on LP8764-Q1 are assigned for this functionality. In addition, the LDOVINT pin of the primary PMIC must be connected to the ENABLE input (GPIO_4 of LP8764-Q1) of the secondary PMIC to correctly initiate the PFSM.

Other digital connections from the TPS6594-Q1 devices to the processor allow support for error monitoring, processor reset, processor wake up, and system low-power modes. Specific GPIO pins have been assigned to key signals in order to ensure proper operation during low power modes when only a few GPIO pins remain operational.

To support DDR retention low power mode, the following PMIC GPIO functions are required:

  1. GPIO_2 and GPIO_3 of LP8764-Q1 connected to an external, low voltage latch to create a sustained control signal to DDR_RET of the processor. The latch is needed since the PMIC VIO_IN power rail supplying GPIO_2 and 3 is disabled during DDR Retention state.
  2. Sustained GPIO_9 of TPS6594-Q1 connected to the enable input of a 3.3V in-line load switch to the MCU.
  3. Sustained GPIO_4 of TPS6594-Q1 with NVM default function set as LP_WKUP1 and mask bit set high to avoid false triggering until CAN wakeup signal is armed. SW must properly arm CAN PHY so that wakeup signal is set high and unmask GPIO_4 before entering GPIO Retention state.
GPIO_4 of TPS6594-Q1 is powered by the VRTC internal voltage domain of the PMIC. The LDOVRTC regulator supplies always-on functions, such as the wake-up function of GPIO_4. This enables GPIO_4 to be used as a wake-up source in LP_STANDBY when LDO_VINT is turned off.

To support GPIO retention low power mode, the following PMIC GPIO functions are required:

  1. Sustained GPIO_7 of LP8764-Q1 connected to the enable input of an in-line load switch to control the 3.3 V GPIO retention domain.

Additional digital options also include GPIO_10 of TPS6594-Q1, which can be configured by software as a 32 kHz clock output for the processor oscillator input (LFOSC ). There is also the option to disable the watchdog timer using hardware, by pulling GPIO_8 of TPS6594-Q1 high. Lastly, GPIO_1 of LP8764-Q1 is included in the power up sequence to enable external regulators, for options such as DDR I/O.

Figure 3-2 TPS6594-Q1 and LP8764-Q1 Digital Connections

The digital connections shown in Figure 3-2 allow system features including MCU-only mode, GPIO retention mode, DDR retention mode, and functional safety systems capable of supporting up to ASIL-D. Please use Table 3-2 as a guide to understand GPIO assignments required for these features. If the feature listed is not required, the digital connection can be removed. For details on how functional safety related connections help achieve functional safety system-level goals, see Section 4.

Table 3-2 Digital Connections by System Feature
DevicePMIC Digital SignalSystem Digital SignalSystem Features
Active SoCFunctional SafetyMCU - onlyGPIO RetentionDDR Retention
TPS6594-Q1nPWRON/ ENABLESystem ON RequestRequired
INT(1)Safety MCU GPIORequired
nRSTOUT(1)MCU_PORzRequiredRequired
SCL_I2C1WKUP_I2C0_SCLRequired
SDA_I2C1WKUP_I2C0_SDARequired
GPIO_1MCU_I2C0_SCLRequired
GPIO_2MCU_I2C0_SCLRequired
GPIO_3SOC_SAFETY_ERRORnOptional
GPIO_4(2)CAN WakeupRequiredRequired
GPIO_5PMIC SPMI CLKRequired
GPIO_6PMIC SPMI DATARequired
GPIO_7MCU_SAFETY_ERRORnOptional
GPIO_8 (5)Disable Watchdog(3)(3)
GPIO_9ENABLE MCU I/ORequired
GPIO_10(4)WKUP_LFOSC0Required
GPIO_11(1)SOC_PORzRequiredRequired
LP8764-Q1INT(1)Safety MCU GPIORequired
SCL_I2C1WKUP_I2C0_SCLRequired
SDA_I2C1WKUP_I2C0_SDARequired
GPIO_1Enable DDR I/O (Optional)
GPIO_2(5)External Latch Data InputRequired
GPIO_3(5)External Latch Clock InputRequired
GPIO_4TPS6594-Q1 LDOVINTRequired
GPIO_5(5)Enable EFUSE
GPIO_6 (5)N/A
GPIO_7EN_GPIO_RETRequiredRequired
GPIO_8PMIC SPMI CLKRequired
GPIO_9PMIC SPMI DATARequired
GPIO_10Enable Main I/ORequiredRequiredRequired
(1) This pin is open-drain to enable voltage translation to correct voltage level for processor interface.
(2) Software must unmask GPIO_4 before the system expects to trigger a wakeup on this pin.
(3) If it is desired to disable the watchdog through hardware, GPIO_8 is required and must be set high by the time nRSTOUT goes high. After nRSTOUT is high, the watchdog state is latched and the pin can be configured for other functions through software.
(4) GPIO_10 is set as a general purpose input (GPI) by default to allow processor to boot up before sourcing the 32 kHz to the processor, since both bootmode and low frequency clock inputs to the processor utilize the same pin.
(5) This GPIO is not required for power sequencing or PMIC functionality and can be configured by software for a different purpose if desired.

4 Supporting Functional Safety Systems

By using the TPS6594-Q1 and LP8764-Q1 solution to power the DRA821 processor, the system can leverage the following PMIC functional safety features:

  • Independent Power Control of MCU and Main Rails
  • Independent Monitoring and Reset for MCU and Main Rails
  • Input Supply Monitoring
  • Output Voltage and Current Monitoring
  • Question & Answer Watchdog
  • Fault Reporting Interrupts
  • Enable Drive Pin that provides an independent path to disable system actuators
  • Error Pin Monitoring
  • Internal Diagnostics including voltage monitoring, temperature monitoring, and Built-In Self-Test

Refer to the Safety Manuals of the TPS6594-Q1 and LP8764-Q1 devices for full descriptions and analysis of the PMIC functional safety features. These functional safety features can assist in achieving up to ASIL-D rating for a system. Additionally, these features help in achieving the functional safety assumptions utilized by the processor to achieve up to ASIL-D rating. See the DRA821 Safety Manual for Jacinto™ 7 Processors for a complete list of functional safety system assumptions.

4.1 Achieving ASIL-B System Requirements

To achieve a system functional safety level of ASIL-B, the following PDN features are available:

  • PMIC over voltage and under voltage monitoring on the power resource voltage outputs
  • PMIC over-voltage monitoring and protection on the input to the PMIC (VCCA)
  • Watchdog monitoring of safety processor
  • MCU error monitoring
  • MCU reset
  • I2C communication
  • Error indicator, EN_DRV, for driving external circuitry (optional)
  • Read-back of EN_DRV pin

The PDN has an in-line, external power FET between the input supply and PMICs. This FET can quickly isolate the PMICs when an over-voltage event greater than 6 V is detected on the input supply to protect the system from being damaged, as shown in Figure 3-1. Note that any power rail connected after the FET can be protected from an over voltage event. Any power connected upstream from the FET is not protected from over voltage events. In Figure 3-1 the load switches that supply power to the MCU and Main I/O domains and the discrete buck supplying the DDR are all connected after the FET to extend the over voltage protection to these processor domains and discrete power resources.

The PMIC internal over voltage and under voltage monitoring and their respective monitoring threshold levels can be enabled through I2C after startup. To monitor the load switch voltage that supplies the MCU I/O of the processor, it is recommended to use the processor POK monitor built into the VDDSHV0_MCU voltage domain.

The PMIC Internal Q&A Watchdog is enabled by default on the TPS6594-Q1 device. Once the device is in ACTIVE state, the trigger or Q&A watchdog settings can be configured through the secondary I2C in the device. The steps for configuring the watchdog settings can be found in the TPS6594-Q1 data sheet. Setting the DISABLE_WDOG signal high on TPS6594-Q1 GPIO_8 disables the watchdog timer if this feature needs to be suspended or is not required in the system.

GPIO_7 of the TPS6594-Q1 PMIC is configured as the MCU error signal monitoring, and must be enabled though the ESM_MCU_EN register bit. MCU reset is supported through the connection between the primary PMIC nRSTOUT pin and the MCU_PORz of the processor. Lastly, there are 2 I2C ports between the TPS6594-Q1 and the processor. The first is used for all non-watchdog communication, such as voltage level control, and the second allows the watchdog monitoring to be on an independent communication channel.

There is an option to use the EN_DRV of theTPS6594-Q1 PMIC to indicate an error has been detected and the system is entering SAFE state. This signal can be utilized if the system has some additional external circuitry that needs to be driven by an error event. In this PDN, the EN_DRV is not utilized, but available if needed.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale